Data Fields
ECDHCC26X2_Object_ Struct Reference

ECDHCC26X2 Object. More...

#include <ECDHCC26X2.h>

Collaboration diagram for ECDHCC26X2_Object_:
Collaboration graph
[legend]

Data Fields

bool isOpen
 
bool operationInProgress
 
bool operationCanceled
 
int_fast16_t operationStatus
 
ECDH_CallbackFxn callbackFxn
 
ECDH_ReturnBehavior returnBehavior
 
ECDH_Operation operation
 
ECDH_OperationType operationType
 
ECDHCC26X2_FsmState fsmState
 
uint32_t semaphoreTimeout
 
uint32_t resultAddress
 

Detailed Description

ECDHCC26X2 Object.

The application must not access any member variables of this structure!

Field Documentation

§ isOpen

bool ECDHCC26X2_Object_::isOpen

§ operationInProgress

bool ECDHCC26X2_Object_::operationInProgress

§ operationCanceled

bool ECDHCC26X2_Object_::operationCanceled

§ operationStatus

int_fast16_t ECDHCC26X2_Object_::operationStatus

§ callbackFxn

ECDH_CallbackFxn ECDHCC26X2_Object_::callbackFxn

§ returnBehavior

ECDH_ReturnBehavior ECDHCC26X2_Object_::returnBehavior

§ operation

ECDH_Operation ECDHCC26X2_Object_::operation

§ operationType

ECDH_OperationType ECDHCC26X2_Object_::operationType

§ fsmState

ECDHCC26X2_FsmState ECDHCC26X2_Object_::fsmState

§ semaphoreTimeout

uint32_t ECDHCC26X2_Object_::semaphoreTimeout

§ resultAddress

uint32_t ECDHCC26X2_Object_::resultAddress

The documentation for this struct was generated from the following file:
© Copyright 1995-2022, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale