ECDHCC26X2.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2017-2018, Texas Instruments Incorporated
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *
9  * * Redistributions of source code must retain the above copyright
10  * notice, this list of conditions and the following disclaimer.
11  *
12  * * Redistributions in binary form must reproduce the above copyright
13  * notice, this list of conditions and the following disclaimer in the
14  * documentation and/or other materials provided with the distribution.
15  *
16  * * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22  * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23  * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24  * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25  * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26  * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27  * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28  * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29  * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30  * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
106 #ifndef ti_drivers_ecdh_ECDHCC26X2__include
107 #define ti_drivers_ecdh_ECDHCC26X2__include
108 
109 #ifdef __cplusplus
110 extern "C" {
111 #endif
112 
113 #include <stdint.h>
114 #include <stdbool.h>
115 
116 #include <ti/drivers/Power.h>
117 #include <ti/drivers/ECDH.h>
120 
121 #include <ti/devices/DeviceFamily.h>
122 #include DeviceFamily_constructPath(driverlib/pka.h)
123 
124 #include <ti/drivers/dpl/HwiP.h>
125 #include <ti/drivers/dpl/SwiP.h>
126 #include <ti/drivers/dpl/SemaphoreP.h>
127 
128 /* Exit the SWI and wait until an HWI call posts the SWI again */
129 #define ECDHCC26X2_STATUS_FSM_RUN_PKA_OP ECDH_STATUS_RESERVED - 0
130 /* Execute the next FSM state immediately without waiting for the next HWI */
131 #define ECDHCC26X2_STATUS_FSM_RUN_FSM ECDH_STATUS_RESERVED - 1
132 
142 typedef enum ECDHCC26X2_FsmState_ {
144 
149 
154 
159 
164 
171 typedef struct ECDHCC26X2_HWAttrs_ {
184  uint8_t intPriority;
186 
192 typedef struct ECDHCC26X2_Object_ {
193  bool isOpen;
196  int_fast16_t operationStatus;
201  ECDHCC26X2_FsmState fsmState;
203  uint32_t resultAddress;
205 
206 #ifdef __cplusplus
207 }
208 #endif
209 
210 #endif /* ti_drivers_ecdh_ECDHCC26X2__include */
ECDH_OperationType
Enum for the operation types supported by the driver.
Definition: ECDH.h:506
bool operationCanceled
Definition: ECDHCC26X2.h:195
int_fast16_t operationStatus
Definition: ECDHCC26X2.h:196
The CryptoKey type is an opaque representation of a cryptographic key.
Definition: ECDHCC26X2.h:143
uint32_t resultAddress
Definition: ECDHCC26X2.h:203
ECDHCC26X2_FsmState fsmState
Definition: ECDHCC26X2.h:201
Power Manager.
ECDH_ReturnBehavior returnBehavior
Definition: ECDHCC26X2.h:198
struct ECDHCC26X2_Object_ ECDHCC26X2_Object
ECDHCC26X2 Object.
ECDH_CallbackFxn callbackFxn
Definition: ECDHCC26X2.h:197
void(* ECDH_CallbackFxn)(ECDH_Handle handle, int_fast16_t returnStatus, ECDH_Operation operation, ECDH_OperationType operationType)
The definition of a callback function used by the ECDH driver when used in ECDH_RETURN_BEHAVIOR_CALLB...
Definition: ECDH.h:529
ECDH_Operation operation
Definition: ECDHCC26X2.h:199
ECDHCC26X2 Hardware Attributes.
Definition: ECDHCC26X2.h:171
TI Driver for Elliptic Curve Diffie-Hellman key agreement scheme.
bool isOpen
Definition: ECDHCC26X2.h:193
ECDHCC26X2_FsmState_
ECDHCC26X2 states.
Definition: ECDHCC26X2.h:142
ECDH_ReturnBehavior
The way in which ECC function calls return after performing an encryption + authentication or decrypt...
Definition: ECDH.h:427
uint8_t intPriority
Crypto Peripheral&#39;s interrupt priority.
Definition: ECDHCC26X2.h:184
uint32_t semaphoreTimeout
Definition: ECDHCC26X2.h:202
ECDH_OperationType operationType
Definition: ECDHCC26X2.h:200
bool operationInProgress
Definition: ECDHCC26X2.h:194
Definition: ECDHCC26X2.h:148
ECDHCC26X2 Object.
Definition: ECDHCC26X2.h:192
struct ECDHCC26X2_HWAttrs_ ECDHCC26X2_HWAttrs
ECDHCC26X2 Hardware Attributes.
enum ECDHCC26X2_FsmState_ ECDHCC26X2_FsmState
ECDHCC26X2 states.
Union containing pointers to all supported operation structs.
Definition: ECDH.h:498
© Copyright 1995-2022, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale