TI BLE Stack API Documentation
2.03.10
|
Functions | |
bStatus_t | GAPBondMgr_SetParameter (uint16 param, uint8 len, void *pValue) |
Set a GAP Bond Manager parameter. More... | |
bStatus_t | GAPBondMgr_GetParameter (uint16 param, void *pValue) |
Get a GAP Bond Manager parameter. More... | |
bStatus_t | GAPBondMgr_LinkEst (uint8 addrType, uint8 *pDevAddr, uint16 connHandle, uint8 role) |
Notify the Bond Manager that a connection has been made. More... | |
void | GAPBondMgr_LinkTerm (uint16 connHandle) |
Notify the Bond Manager that a connection has been terminated. More... | |
void | GAPBondMgr_SlaveReqSecurity (uint16 connHandle, uint8 authReq) |
uint8 | GAPBondMgr_ResolveAddr (uint8 addrType, uint8 *pDevAddr, uint8 *pResolvedAddr) |
Resolve an address from bonding information. More... | |
bStatus_t | GAPBondMgr_ServiceChangeInd (uint16 connectionHandle, uint8 setParam) |
Set/clear the service change indication in a bond record. More... | |
bStatus_t | GAPBondMgr_UpdateCharCfg (uint16 connectionHandle, uint16 attrHandle, uint16 value) |
Update the Characteristic Configuration in a bond record. More... | |
void | GAPBondMgr_Register (gapBondCBs_t *pCB) |
Register callback functions with the bond manager. More... | |
bStatus_t | GAPBondMgr_PasscodeRsp (uint16 connectionHandle, uint8 status, uint32 passcode) |
Respond to a passcode request. More... | |
bStatus_t | GAPBondMgr_ReadCentAddrResChar (uint16 connectionHandle) |
Send Read By Type Request to get value attribute of Central Address Resolution characteristic. Value determines if peer supports Enhanced Privacy. Bond record will automatically be updated based on peer response. More... | |
uint8 | GAPBondMgr_SupportsEnhancedPriv (uint8 *pPeerIdAddr) |
Determine if peer device supports enhanced privacy by checking the Enhanced Privacy state flag of the bond record that corresponds to the peer's identity address. More... | |
uint8 | GAPBondMgr_ProcessGAPMsg (gapEventHdr_t *pMsg) |
This is a bypass mechanism to allow the bond manager to process GAP messages. More... | |
uint8 | GAPBondMgr_CheckNVLen (uint8 id, uint8 len) |
This function will check the length of a Bond Manager NV Item. More... | |
bStatus_t | GAPBondMgr_syncResolvingList (void) |
This function will add all device address and IRK pairs from bond records to the Controller. Used with PRIVACY_1_2_CFG. More... | |
uint8 GAPBondMgr_CheckNVLen | ( | uint8 | id, |
uint8 | len | ||
) |
This function will check the length of a Bond Manager NV Item.
id | - NV ID. |
len | - lengths in bytes of item. |
bStatus_t GAPBondMgr_GetParameter | ( | uint16 | param, |
void * | pValue | ||
) |
Get a GAP Bond Manager parameter.
NOTE: You can call this function with a GAP Parameter ID and it will get a GAP Parameter. GAP Parameters are defined in (gap.h). Also, the "pValue" field must point to a "uint16".
param | - Profile parameter ID: GAP Bond Manager Parameters |
pValue | - pointer to location to get the value. This is dependent on the parameter ID and WILL be cast to the appropriate data type (example: data type of uint16 will be cast to uint16 pointer). |
bStatus_t GAPBondMgr_LinkEst | ( | uint8 | addrType, |
uint8 * | pDevAddr, | ||
uint16 | connHandle, | ||
uint8 | role | ||
) |
Notify the Bond Manager that a connection has been made.
NOTE: The GAP Peripheral/Central Role profile will call this function, if they are included in the project.
addrType | - device's address type. Reference ADDRTYPE_DEFINES in gap.h |
pDevAddr | - device's address |
connHandle | - connection handle |
role | - master or slave role. Reference GAP_PROFILE_ROLE_DEFINES in gap.h |
void GAPBondMgr_LinkTerm | ( | uint16 | connHandle | ) |
Notify the Bond Manager that a connection has been terminated.
NOTE: The GAP Peripheral/Central Role profile will call this function, if they are included in the project.
connHandle | - connection handle |
bStatus_t GAPBondMgr_PasscodeRsp | ( | uint16 | connectionHandle, |
uint8 | status, | ||
uint32 | passcode | ||
) |
Respond to a passcode request.
connectionHandle | - connection handle of the connected device or 0xFFFF if all devices in database. |
status | - SUCCESS if passcode is available, otherwise see Pairing failure status values. |
passcode | - integer value containing the passcode. |
uint8 GAPBondMgr_ProcessGAPMsg | ( | gapEventHdr_t * | pMsg | ) |
This is a bypass mechanism to allow the bond manager to process GAP messages.
NOTE: This is an advanced feature and shouldn't be called unless the normal GAP Bond Manager task ID registration is overridden.
pMsg | - GAP event message |
bStatus_t GAPBondMgr_ReadCentAddrResChar | ( | uint16 | connectionHandle | ) |
Send Read By Type Request to get value attribute of Central Address Resolution characteristic. Value determines if peer supports Enhanced Privacy. Bond record will automatically be updated based on peer response.
connectionHandle | - connection handle of the connected device |
void GAPBondMgr_Register | ( | gapBondCBs_t * | pCB | ) |
Register callback functions with the bond manager.
NOTE: There is no need to register a passcode callback function if the passcode will be handled with the GAPBOND_DEFAULT_PASSCODE parameter.
pCB | - pointer to callback function structure. |
uint8 GAPBondMgr_ResolveAddr | ( | uint8 | addrType, |
uint8 * | pDevAddr, | ||
uint8 * | pResolvedAddr | ||
) |
Resolve an address from bonding information.
addrType | - peer's address type. Reference ADDRTYPE_DEFINES in gap.h |
pDevAddr | - peer's address |
pResolvedAddr | - pointer to buffer to put the resolved address |
bStatus_t GAPBondMgr_ServiceChangeInd | ( | uint16 | connectionHandle, |
uint8 | setParam | ||
) |
Set/clear the service change indication in a bond record.
connectionHandle | - connection handle of the connected device or 0xFFFF if all devices in database. |
setParam | - TRUE to set the service change indication, FALSE to clear it. |
bStatus_t GAPBondMgr_SetParameter | ( | uint16 | param, |
uint8 | len, | ||
void * | pValue | ||
) |
Set a GAP Bond Manager parameter.
NOTE: You can call this function with a GAP Parameter ID and it will set the GAP Parameter. GAP Parameters are defined in (gap.h). Also, the "len" field must be set to the size of a "uint16" and the "pValue" field must point to a "uint16".
param | - Profile parameter ID: GAP Bond Manager Parameters |
len | - length of data to write |
pValue | - pointer to data to write. This is dependent on the parameter ID and WILL be cast to the appropriate data type (example: data type of uint16 will be cast to uint16 pointer). |
uint8 GAPBondMgr_SupportsEnhancedPriv | ( | uint8 * | pPeerIdAddr | ) |
Determine if peer device supports enhanced privacy by checking the Enhanced Privacy state flag of the bond record that corresponds to the peer's identity address.
pPeerIdAddr | - peer identity address |
bStatus_t GAPBondMgr_syncResolvingList | ( | void | ) |
This function will add all device address and IRK pairs from bond records to the Controller. Used with PRIVACY_1_2_CFG.
none |
bStatus_t GAPBondMgr_UpdateCharCfg | ( | uint16 | connectionHandle, |
uint16 | attrHandle, | ||
uint16 | value | ||
) |
Update the Characteristic Configuration in a bond record.
connectionHandle | - connection handle of the connected device or 0xFFFF if all devices in database. |
attrHandle | - attribute handle. |
value | - characteristic configuration value. |