![]() |
![]() |
#include <vcd.h>
Data Fields | |
VCD_RecoResultEnum | status |
int_least32_t | fullScore |
int_least32_t | confScore |
int_least16_t | normScore |
int_least16_t | modelIndex |
char const * | name |
A structure that holds the results of recognition. The structure is filled by calling VCD_getResult.
VCD_RecoResultEnum VCD_RecoStructDef::status |
The recognition result status. See VCD_RecoResultEnum
int_least32_t VCD_RecoStructDef::fullScore |
Full accumulated score over all processed frames
int_least32_t VCD_RecoStructDef::confScore |
Confidence measure score - larger is more confident
int_least16_t VCD_RecoStructDef::normScore |
Normalized score for current frame relative to best state score
int_least16_t VCD_RecoStructDef::modelIndex |
Model index recognized, if any. May be less than zero if the best hypothesis indicates a silence or filler model
char const* VCD_RecoStructDef::name |
Word corresponding to recognized result, if any