xWRL6432 MMWAVE-L-SDK  05.05.00.00

Introduction

Macros that define the compression method.

Value Mode
0 EGE Compression/Decompression
1 BFP Block floating point algorithm

Macros

#define HWA_COMPRESS_METHOD_EGE   ((uint8_t)0U)
 
#define HWA_COMPRESS_METHOD_BFP   ((uint8_t)1U)
 

Macro Definition Documentation

◆ HWA_COMPRESS_METHOD_EGE

#define HWA_COMPRESS_METHOD_EGE   ((uint8_t)0U)

Exponential Golomb Encoder Compression.

◆ HWA_COMPRESS_METHOD_BFP

#define HWA_COMPRESS_METHOD_BFP   ((uint8_t)1U)

Block Floating point algorithm