![Logo](ti_logo.svg) |
xWRL6432 MMWAVE-L-SDK
05.05.00.00
|
|
Go to the documentation of this file.
43 #ifndef DOPPLERPROC_INTERNAL_H_
44 #define DOPPLERPROC_INTERNAL_H_
78 typedef struct DPU_DopplerProcHWA_Obj_t
SemaphoreP_Object edmaDoneSemaHandle
EDMA Done semaphore Handle.
Definition: dopplerproc_internal.h:93
DPU_DopplerProc_Edma edmaIn
EDMA configuration for Input data (Radar cube -> HWA memory).
Definition: dopplerproc_internal.h:87
EDMA_Handle edmaHandle
EDMA driver handle.
Definition: dopplerproc_internal.h:84
dopplerProc DPU internal data Object
Definition: dopplerproc_internal.h:79
Defines the detection matrix buffer interface.
uint8_t hwaDmaTriggerSourcePong
DMA trigger source channel for Pong param set.
Definition: dopplerproc_internal.h:102
Base error codes for the data path Modules.
Implements Datapath doppler processing functionality using the HWA. Based on the RF parameters and ra...
dopplerProc DPU EDMA configuration parameters
Definition: dopplerproc_common.h:70
uint8_t hwaDmaTriggerSourcePing
DMA trigger source channel for Ping param set.
Definition: dopplerproc_internal.h:99
uint16_t hwaNumLoops
HWA number of loops.
Definition: dopplerproc_internal.h:105
SemaphoreP_Object hwaDoneSemaHandle
HWA Processing Done semaphore Handle.
Definition: dopplerproc_internal.h:90
#define DPU_DOPPLERPROCHWA_NUM_HWA_MEMBANKS
Number of HWA memory banks needed.
Definition: dopplerprochwa.h:166
Defines the data path radar cube data interface.
void * EDMA_Handle
A handle that is returned from a EDMA_open() call.
Definition: edma/v0/edma.h:471
HWA_Handle hwaHandle
HWA Handle.
Definition: dopplerproc_internal.h:81
Opaque semaphore object used with the semaphore APIs.
Definition: SemaphoreP.h:59
uint8_t hwaParamStopIdx
HWA stop paramset index.
Definition: dopplerproc_internal.h:111
uint8_t hwaParamStartIdx
HWA start paramset index.
Definition: dopplerproc_internal.h:108
bool inProgress
Flag to indicate if DPU is in processing state.
Definition: dopplerproc_internal.h:96
void * HWA_Handle
A handle that is returned from a HWA_open() call.
Definition: hwa/v0/hwa.h:612