HWA Debug statistics.
HWA debug - current paramset, loopcount, trigger status - that are output from the statistics block.
Data Fields | |
uint8_t | currentParamSet |
uint16_t | currentLoopCount |
uint16_t | dmaTrigStatus |
uint8_t | dfePingPongStatus |
uint8_t | swTrigStatus |
uint8_t HWA_DebugStats::currentParamSet |
Index of the current paramset that is under execution. useful for debug, where parameter-sets can be executed one-by-one using SW trigger mode for each of them. In such a debug, this register indicates which parameter-set is currently waiting for the SW trigger
uint16_t HWA_DebugStats::currentLoopCount |
the loop count that is presently running
uint16_t HWA_DebugStats::dmaTrigStatus |
indicates whether a trigger was received via DMA trigger method
uint8_t HWA_DebugStats::dfePingPongStatus |
the status of DFE ping-pong trigger
uint8_t HWA_DebugStats::swTrigStatus |
the status of software trigger