Macros that define values for the trigger mode of HWA paramsets.
Macros | |
#define | HWA_TRIG_MODE_IMMEDIATE ((uint8_t)0U) |
#define | HWA_TRIG_MODE_SOFTWARE ((uint8_t)1U) |
#define | HWA_TRIG_MODE_RESERVED1 ((uint8_t)2U) |
#define | HWA_TRIG_MODE_DMA ((uint8_t)3U) |
#define | HWA_TRIG_MODE_HARDWARE ((uint8_t)4U) |
#define | HWA_TRIG_MODE_RESERVED2 ((uint8_t)5U) |
#define | HWA_TRIG_MODE_RESERVED3 ((uint8_t)6U) |
#define | HWA_TRIG_MODE_M4CONTROL ((uint8_t)7U) |
#define HWA_TRIG_MODE_IMMEDIATE ((uint8_t)0U) |
state machine reads and immediately executes that paramset
#define HWA_TRIG_MODE_SOFTWARE ((uint8_t)1U) |
state machine reads the paramset but waits for s/w trigger before executing that paramset
#define HWA_TRIG_MODE_RESERVED1 ((uint8_t)2U) |
Reserved
#define HWA_TRIG_MODE_DMA ((uint8_t)3U) |
state machine reads the paramset but waits for DMA trigger before executing that paramset
#define HWA_TRIG_MODE_HARDWARE ((uint8_t)4U) |
Hardware based trigger #1
#define HWA_TRIG_MODE_RESERVED2 ((uint8_t)5U) |
Hardware based trigger #2
#define HWA_TRIG_MODE_RESERVED3 ((uint8_t)6U) |
Hardware based trigger #3
#define HWA_TRIG_MODE_M4CONTROL ((uint8_t)7U) |
equivalent to software trigger, M4 Micro-controller based trigger