Macros that define values for the ramType argument of HWA_configRam() function.
Macros | |
#define | HWA_RAM_TYPE_WINDOW_RAM ((uint8_t)0U) |
#define | HWA_RAM_TYPE_INTERNAL_RAM ((uint8_t)1U) |
#define HWA_RAM_TYPE_WINDOW_RAM ((uint8_t)0U) |
WINDOW RAM for windowing operation
#define HWA_RAM_TYPE_INTERNAL_RAM ((uint8_t)1U) |
Internal RAM for Vector Multiplication mode