Enable/Disable for Interference zeroing-out This register bit controls the enable/disable for the interference zero-ing feature. The feature is enabled if this register bit is set to 1.
Macros | |
#define | HWA_INTERFERENCE_ENABLE ((uint8_t)1U) |
#define | HWA_INTERFERENCE_DISABLE ((uint8_t)0U) |
#define HWA_INTERFERENCE_ENABLE ((uint8_t)1U) |
#define HWA_INTERFERENCE_DISABLE ((uint8_t)0U) |