Macros that define values for the selecting either the compression or the decompression mode of CMP_DCMP_Engine.
Value | Mode |
---|---|
0 | Compression |
1 | Decompression |
Macros | |
#define | HWA_CMP_DCMP_COMPRESS ((uint8_t)0U) |
#define | HWA_CMP_DCMP_DECOMPRESS ((uint8_t)1U) |
#define HWA_CMP_DCMP_COMPRESS ((uint8_t)0U) |
Compression mode.
#define HWA_CMP_DCMP_DECOMPRESS ((uint8_t)1U) |
Decompression mode.