Macros that define the compression method.
Value | Mode |
---|---|
0 | EGE Compression/Decompression |
1 | BFP Block floating point algorithm |
Macros | |
#define | HWA_COMPRESS_METHOD_EGE ((uint8_t)0U) |
#define | HWA_COMPRESS_METHOD_BFP ((uint8_t)1U) |
#define HWA_COMPRESS_METHOD_EGE ((uint8_t)0U) |
Exponential Golomb Encoder Compression.
#define HWA_COMPRESS_METHOD_BFP ((uint8_t)1U) |
Block Floating point algorithm