This module contains APIs to program and use the UART.
Files | |
file | uart_sci.h |
This file contains the prototype of UART driver APIs. | |
Data Structures | |
struct | UART_Transaction |
Data structure used with UART_read() and UART_write() More... | |
struct | UART_Params |
UART Parameters. More... | |
struct | UART_Attrs |
UART instance attributes - used during init time. More... | |
struct | UART_EdmaParams |
UART EDMA Parameters. More... | |
struct | UART_Object |
UART driver object. More... | |
struct | UART_Config |
UART global configuration array. More... | |
Functions | |
void | UART_init (void) |
This function initializes the UART module. More... | |
void | UART_deinit (void) |
This function de-initializes the UART module. More... | |
UART_Handle | UART_open (uint32_t index, const UART_Params *prms) |
This function opens a given UART peripheral. More... | |
void | UART_close (UART_Handle handle) |
Function to close a UART peripheral specified by the UART handle. More... | |
int32_t | UART_write (UART_Handle handle, UART_Transaction *trans) |
Function to perform UART write operation. More... | |
int32_t | UART_read (UART_Handle handle, UART_Transaction *trans) |
Function to perform UART read operation. More... | |
int32_t | UART_writeCancel (UART_Handle handle, UART_Transaction *trans) |
Function to perform UART canceling of current write transaction. More... | |
int32_t | UART_readCancel (UART_Handle handle, UART_Transaction *trans) |
Function to perform UART canceling of current read transaction. More... | |
UART_Handle | UART_getHandle (uint32_t index) |
Function to return a open'ed UART handle given a UART instance index. More... | |
void | UART_flushTxFifo (UART_Handle handle) |
Function to flush a TX FIFO of peripheral specified by the UART handle. More... | |
static void | UART_Params_init (UART_Params *prms) |
Function to initialize the UART_Params struct to its defaults. More... | |
static void | UART_Transaction_init (UART_Transaction *trans) |
Function to initialize the UART_Transaction struct to its defaults. More... | |
Typedefs | |
typedef void * | UART_Handle |
A handle that is returned from a UART_open() call. More... | |
typedef void(* | UART_CallbackFxn) (UART_Handle handle, UART_Transaction *transaction) |
The definition of a callback function used by the UART driver when used in UART_TRANSFER_MODE_CALLBACK. More... | |
Transfer Status Code | |
Status codes that are set by the UART driver | |
#define | UART_TRANSFER_STATUS_SUCCESS (0U) |
Transaction success. More... | |
#define | UART_TRANSFER_STATUS_TIMEOUT (1U) |
Time out error. More... | |
#define | UART_TRANSFER_STATUS_ERROR_BI (2U) |
Break condition error. More... | |
#define | UART_TRANSFER_STATUS_ERROR_FE (3U) |
Framing error. More... | |
#define | UART_TRANSFER_STATUS_ERROR_PE (4U) |
Parity error. More... | |
#define | UART_TRANSFER_STATUS_ERROR_OE (5U) |
Overrun error. More... | |
#define | UART_TRANSFER_STATUS_CANCELLED (6U) |
Cancelled. More... | |
#define | UART_TRANSFER_STATUS_STARTED (7U) |
Transaction started. More... | |
#define | UART_TRANSFER_STATUS_READ_TIMEOUT (8U) |
Read timeout error. More... | |
#define | UART_TRANSFER_STATUS_ERROR_INUSE (9U) |
UART is currently in use. More... | |
#define | UART_TRANSFER_STATUS_ERROR_OTH (10U) |
Other errors. More... | |
Transfer Mode | |
This determines whether the driver operates synchronously or asynchronously In UART_TRANSFER_MODE_BLOCKING mode UART_read() and UART_write() blocks code execution until the transaction has completed In UART_TRANSFER_MODE_CALLBACK UART_read() and UART_write() does not block code execution and instead calls a UART_CallbackFxn callback function when the transaction has completed | |
#define | UART_TRANSFER_MODE_BLOCKING (0U) |
UART read/write APIs blocks execution. This mode can only be used when called within a Task context. More... | |
#define | UART_TRANSFER_MODE_CALLBACK (1U) |
UART read/write APIs does not block code execution and will call a UART_CallbackFxn. This mode can be used in a Task, Swi, or Hwi context. More... | |
UART data length | |
Note: The values should not be changed since it represents the actual register configuration values used to configure the UART | |
#define | UART_LEN_1 (0U) |
#define | UART_LEN_2 (1U) |
#define | UART_LEN_3 (2U) |
#define | UART_LEN_4 (3U) |
#define | UART_LEN_5 (4U) |
#define | UART_LEN_6 (5U) |
#define | UART_LEN_7 (6U) |
#define | UART_LEN_8 (7U) |
UART stop bits | |
Note: The values should not be changed since it represents the actual register configuration values used to configure the UART | |
#define | UART_STOPBITS_1 (0U) |
#define | UART_STOPBITS_2 (1U) |
UART Parity | |
Note: The values should not be changed since it represents the actual register configuration values used to configure the UART | |
#define | UART_PARITY_NONE (0x00U) |
#define | UART_PARITY_ODD (0x01U) |
#define | UART_PARITY_EVEN (0x03U) |
UART Configration Mode | |
This determines whether the driver configuration mode like Polled, Interrupt, Dma used for the transfer function | |
#define | UART_CONFIG_MODE_POLLED (0x00U) |
#define | UART_CONFIG_MODE_INTERRUPT (0x01U) |
#define | UART_CONFIG_MODE_USER_INTR (0x02U) |
#define | UART_CONFIG_MODE_DMA (0x03U) |
#define UART_TRANSFER_STATUS_SUCCESS (0U) |
Transaction success.
#define UART_TRANSFER_STATUS_TIMEOUT (1U) |
Time out error.
#define UART_TRANSFER_STATUS_ERROR_BI (2U) |
Break condition error.
#define UART_TRANSFER_STATUS_ERROR_FE (3U) |
Framing error.
#define UART_TRANSFER_STATUS_ERROR_PE (4U) |
Parity error.
#define UART_TRANSFER_STATUS_ERROR_OE (5U) |
Overrun error.
#define UART_TRANSFER_STATUS_CANCELLED (6U) |
Cancelled.
#define UART_TRANSFER_STATUS_STARTED (7U) |
Transaction started.
#define UART_TRANSFER_STATUS_READ_TIMEOUT (8U) |
Read timeout error.
#define UART_TRANSFER_STATUS_ERROR_INUSE (9U) |
UART is currently in use.
#define UART_TRANSFER_STATUS_ERROR_OTH (10U) |
Other errors.
#define UART_TRANSFER_MODE_BLOCKING (0U) |
UART read/write APIs blocks execution. This mode can only be used when called within a Task context.
#define UART_TRANSFER_MODE_CALLBACK (1U) |
UART read/write APIs does not block code execution and will call a UART_CallbackFxn. This mode can be used in a Task, Swi, or Hwi context.
#define UART_LEN_1 (0U) |
#define UART_LEN_2 (1U) |
#define UART_LEN_3 (2U) |
#define UART_LEN_4 (3U) |
#define UART_LEN_5 (4U) |
#define UART_LEN_6 (5U) |
#define UART_LEN_7 (6U) |
#define UART_LEN_8 (7U) |
#define UART_STOPBITS_1 (0U) |
#define UART_STOPBITS_2 (1U) |
#define UART_PARITY_NONE (0x00U) |
#define UART_PARITY_ODD (0x01U) |
#define UART_PARITY_EVEN (0x03U) |
#define UART_CONFIG_MODE_POLLED (0x00U) |
#define UART_CONFIG_MODE_INTERRUPT (0x01U) |
#define UART_CONFIG_MODE_USER_INTR (0x02U) |
#define UART_CONFIG_MODE_DMA (0x03U) |
typedef void* UART_Handle |
A handle that is returned from a UART_open() call.
typedef void(* UART_CallbackFxn) (UART_Handle handle, UART_Transaction *transaction) |
The definition of a callback function used by the UART driver when used in UART_TRANSFER_MODE_CALLBACK.
handle | UART_Handle |
transaction | Pointer to a UART_Transaction |
void UART_init | ( | void | ) |
This function initializes the UART module.
void UART_deinit | ( | void | ) |
This function de-initializes the UART module.
UART_Handle UART_open | ( | uint32_t | index, |
const UART_Params * | prms | ||
) |
This function opens a given UART peripheral.
index | Index of config to use in the UART_Config array |
prms | Pointer to open parameters. If NULL is passed, then default values will be used |
void UART_close | ( | UART_Handle | handle | ) |
Function to close a UART peripheral specified by the UART handle.
handle | UART_Handle returned from UART_open() |
int32_t UART_write | ( | UART_Handle | handle, |
UART_Transaction * | trans | ||
) |
Function to perform UART write operation.
In UART_TRANSFER_MODE_BLOCKING, UART_write() will block task execution until the transaction has completed or a timeout has occurred.
In UART_TRANSFER_MODE_CALLBACK, UART_write() does not block task execution, but calls a UART_CallbackFxn once the transfer has finished. This makes UART_write() safe to be used within a Task, software or hardware interrupt context.
From calling UART_write() until transfer completion, the UART_Transaction structure must stay persistent and must not be altered by application code. It is also forbidden to modify the content of the UART_Transaction.buf during a transaction, even though the physical transfer might not have started yet. Doing this can result in data corruption.
handle | UART_Handle returned from UART_open() |
trans | Pointer to a UART_Transaction. All of the fields within transaction except UART_Transaction.count and UART_Transaction.status are WO (write-only) unless otherwise noted in the driver implementations. If a transaction timeout has occurred, UART_Transaction.count will contain the number of bytes that were transferred. Neither is it allowed to modify the transaction object nor the content of UART_Transaction.buf until the transfer has completed |
int32_t UART_read | ( | UART_Handle | handle, |
UART_Transaction * | trans | ||
) |
Function to perform UART read operation.
In UART_TRANSFER_MODE_BLOCKING, UART_read() will block task execution until the transaction has completed or a timeout has occurred.
In UART_TRANSFER_MODE_CALLBACK, UART_read() does not block task execution, but calls a UART_CallbackFxn once the transfer has finished. This makes UART_read() safe to be used within a Task, software or hardware interrupt context.
From calling UART_read() until transfer completion, the UART_Transaction structure must stay persistent and must not be altered by application code. It is also forbidden to modify the content of the UART_Transaction.buf during a transaction, even though the physical transfer might not have started yet. Doing this can result in data corruption.
handle | UART_Handle returned from UART_open() |
trans | Pointer to a UART_Transaction. All of the fields within transaction except UART_Transaction.count and UART_Transaction.status are WO (write-only) unless otherwise noted in the driver implementations. If a transaction timeout has occurred, UART_Transaction.count will contain the number of bytes that were transferred. Neither is it allowed to modify the transaction object nor the content of UART_Transaction.buf until the transfer has completed |
int32_t UART_writeCancel | ( | UART_Handle | handle, |
UART_Transaction * | trans | ||
) |
Function to perform UART canceling of current write transaction.
In UART_TRANSFER_MODE_CALLBACK, UART_writeCancel() does not block task execution, but calls a UART_CallbackFxn once the cancel has finished. This makes UART_writeCancel() safe to be used within a Task, software or hardware interrupt context.
From calling UART_writeCancel() until cancel completion, the UART_Transaction structure must stay persistent and must not be altered by application code. It is also forbidden to modify the content of the UART_Transaction.buf during a transaction, even though the physical transfer might not have started yet. Doing this can result in data corruption.
handle | UART_Handle returned from UART_open() |
trans | Pointer to a UART_Transaction. All of the fields within transaction except UART_Transaction.count and UART_Transaction.status are WO (write-only) unless otherwise noted in the driver implementations. If a transaction timeout has occurred, UART_Transaction.count will contain the number of bytes that were transferred. Neither is it allowed to modify the transaction object nor the content of UART_Transaction.buf until the transfer has completed |
int32_t UART_readCancel | ( | UART_Handle | handle, |
UART_Transaction * | trans | ||
) |
Function to perform UART canceling of current read transaction.
In UART_TRANSFER_MODE_CALLBACK, UART_readCancel() does not block task execution, but calls a UART_CallbackFxn once the cancel has finished. This makes UART_writeCancel() safe to be used within a Task, software or hardware interrupt context.
From calling UART_readCancel() until cancel completion, the UART_Transaction structure must stay persistent and must not be altered by application code. It is also forbidden to modify the content of the UART_Transaction.buf during a transaction, even though the physical transfer might not have started yet. Doing this can result in data corruption.
handle | UART_Handle returned from UART_open() |
trans | Pointer to a UART_Transaction. All of the fields within transaction except UART_Transaction.count and UART_Transaction.status are WO (write-only) unless otherwise noted in the driver implementations. If a transaction timeout has occurred, UART_Transaction.count will contain the number of bytes that were transferred. Neither is it allowed to modify the transaction object nor the content of UART_Transaction.buf until the transfer has completed |
UART_Handle UART_getHandle | ( | uint32_t | index | ) |
Function to return a open'ed UART handle given a UART instance index.
index | Index of config to use in the UART_Config array |
void UART_flushTxFifo | ( | UART_Handle | handle | ) |
Function to flush a TX FIFO of peripheral specified by the UART handle.
handle | UART_Handle returned from UART_open() |
|
inlinestatic |
Function to initialize the UART_Params struct to its defaults.
prms | Pointer to UART_Params structure for initialization |
|
inlinestatic |
Function to initialize the UART_Transaction struct to its defaults.
trans | Pointer to UART_Transaction structure for initialization |
|
extern |
Externally defined driver configuration array.
|
extern |
Externally defined driver configuration array size.