The section has a list of all the error codes which are generated by the sampleProc DPU.
Base error code for the rangeProc DPU is defined in the
Macros | |
| #define | DPU_RANGEPROCHWA_EINVAL (DP_ERRNO_RANGE_PROC_BASE-1) |
| Error Code: Invalid argument. More... | |
| #define | DPU_RANGEPROCHWA_ENOMEM (DP_ERRNO_RANGE_PROC_BASE-2) |
| Error Code: Out of memory. More... | |
| #define | DPU_RANGEPROCHWA_EINTERNAL (DP_ERRNO_RANGE_PROC_BASE-3) |
| Error Code: Internal error. More... | |
| #define | DPU_RANGEPROCHWA_ENOTIMPL (DP_ERRNO_RANGE_PROC_BASE-4) |
| Error Code: Not implemented. More... | |
| #define | DPU_RANGEPROCHWA_EINPROGRESS (DP_ERRNO_RANGE_PROC_BASE-5) |
| Error Code: In Progress. More... | |
| #define | DPU_RANGEPROCHWA_ECMD (DP_ERRNO_RANGE_PROC_BASE-6) |
| Error Code: Invalid control command. More... | |
| #define | DPU_RANGEPROCHWA_ESEMA (DP_ERRNO_RANGE_PROC_BASE-7) |
| Error Code: Semaphore error. More... | |
| #define | DPU_RANGEPROCHWA_EDCREMOVAL (DP_ERRNO_RANGE_PROC_BASE-8) |
| Error Code: DC range signal removal configuration error. More... | |
| #define | DPU_RANGEPROCHWA_EADCBUF_INTF (DP_ERRNO_RANGE_PROC_BASE-9) |
| Error Code: ADCBuf data interface configuration error. More... | |
| #define | DPU_RANGEPROCHWA_ERADARCUBE_INTF (DP_ERRNO_RANGE_PROC_BASE-10) |
| Error Code: ADCBuf data interface configuration error. More... | |
| #define | DPU_RANGEPROCHWA_EWINDOW (DP_ERRNO_RANGE_PROC_BASE-11) |
| Error Code: HWA windowing configuration error. More... | |
| #define | DPU_RANGEPROCHWA_EBUTTERFLYSCALE (DP_ERRNO_RANGE_PROC_BASE-12) |
| Error Code: Incorrect number of butterfly stages specified for scaling. More... | |
| #define | DPU_RANGEPROCHWA_EEDMA_ERROR (DP_ERRNO_RANGE_PROC_BASE-13) |
| Error Code: Incorrect number of butterfly stages specified for scaling. More... | |
| #define DPU_RANGEPROCHWA_EINVAL (DP_ERRNO_RANGE_PROC_BASE-1) |
Error Code: Invalid argument.
| #define DPU_RANGEPROCHWA_ENOMEM (DP_ERRNO_RANGE_PROC_BASE-2) |
Error Code: Out of memory.
| #define DPU_RANGEPROCHWA_EINTERNAL (DP_ERRNO_RANGE_PROC_BASE-3) |
Error Code: Internal error.
| #define DPU_RANGEPROCHWA_ENOTIMPL (DP_ERRNO_RANGE_PROC_BASE-4) |
Error Code: Not implemented.
| #define DPU_RANGEPROCHWA_EINPROGRESS (DP_ERRNO_RANGE_PROC_BASE-5) |
Error Code: In Progress.
| #define DPU_RANGEPROCHWA_ECMD (DP_ERRNO_RANGE_PROC_BASE-6) |
Error Code: Invalid control command.
| #define DPU_RANGEPROCHWA_ESEMA (DP_ERRNO_RANGE_PROC_BASE-7) |
Error Code: Semaphore error.
| #define DPU_RANGEPROCHWA_EDCREMOVAL (DP_ERRNO_RANGE_PROC_BASE-8) |
Error Code: DC range signal removal configuration error.
| #define DPU_RANGEPROCHWA_EADCBUF_INTF (DP_ERRNO_RANGE_PROC_BASE-9) |
Error Code: ADCBuf data interface configuration error.
| #define DPU_RANGEPROCHWA_ERADARCUBE_INTF (DP_ERRNO_RANGE_PROC_BASE-10) |
Error Code: ADCBuf data interface configuration error.
| #define DPU_RANGEPROCHWA_EWINDOW (DP_ERRNO_RANGE_PROC_BASE-11) |
Error Code: HWA windowing configuration error.
| #define DPU_RANGEPROCHWA_EBUTTERFLYSCALE (DP_ERRNO_RANGE_PROC_BASE-12) |
Error Code: Incorrect number of butterfly stages specified for scaling.
| #define DPU_RANGEPROCHWA_EEDMA_ERROR (DP_ERRNO_RANGE_PROC_BASE-13) |
Error Code: Incorrect number of butterfly stages specified for scaling.