Base error code for the dopplerProc DPU is defined in the
Macros | |
#define | DPU_DOAPROC_EINVAL (DP_ERRNO_DOA_PROC_BASE-1) |
Error Code: Invalid argument. More... | |
#define | DPU_DOAPROC_ENOMEM (DP_ERRNO_DOA_PROC_BASE-2) |
Error Code: Out of memory. More... | |
#define | DPU_DOAPROC_EINPROGRESS (DP_ERRNO_DOA_PROC_BASE-3) |
Error Code: DPU is in progress. More... | |
#define | DPU_DOAPROC_EHWARES (DP_ERRNO_DOA_PROC_BASE-4) |
Error Code: Out of HWA resources. More... | |
#define | DPU_DOAPROC_ESEMA (DP_ERRNO_DOA_PROC_BASE-5) |
Error Code: Semaphore creation failed. More... | |
#define | DPU_DOAPROC_ESEMASTATUS (DP_ERRNO_DOA_PROC_BASE-6) |
Error Code: Bad semaphore status. More... | |
#define | DPU_DOAPROC_EEXCEEDHWAMEM (DP_ERRNO_DOA_PROC_BASE-7) |
Error Code: Configure parameters exceed HWA memory bank size. More... | |
#define | DPU_DOAPROC_ECUBEFORMAT (DP_ERRNO_DOA_PROC_BASE-8) |
Error Code: Unsupported radar cube format. More... | |
#define | DPU_DOAPROC_EDETMFORMAT (DP_ERRNO_DOA_PROC_BASE-9) |
Error Code: Unsupported detection matrix format. More... | |
#define | DPU_DOAPROC_EDETMSIZE (DP_ERRNO_DOA_PROC_BASE-10) |
Error Code: Insufficient detection matrix size. More... | |
#define | DPU_DOAPROC_EWINDSIZE (DP_ERRNO_DOA_PROC_BASE-11) |
Error Code: Wrong window size. More... | |
#define | DPU_DOAPROC_E_NOTSUPPORTED_ANGLE_DIM_ONE_AND_CPU_LOOP_CTRL (DP_ERRNO_DOA_PROC_BASE-12) |
Error Code: Not supported angle dim 1 (no elevation) and. More... | |
#define | DPU_DOAPROC_E_EXCEEDED_MAX_NUM_DOPPLER_BINS (DP_ERRNO_DOA_PROC_BASE-13) |
Error Code: Doppler FFT size exceeded the limit. Maximum Doppler index is stored in array of type uint8_t. More... | |
#define DPU_DOAPROC_EINVAL (DP_ERRNO_DOA_PROC_BASE-1) |
Error Code: Invalid argument.
#define DPU_DOAPROC_ENOMEM (DP_ERRNO_DOA_PROC_BASE-2) |
Error Code: Out of memory.
#define DPU_DOAPROC_EINPROGRESS (DP_ERRNO_DOA_PROC_BASE-3) |
Error Code: DPU is in progress.
#define DPU_DOAPROC_EHWARES (DP_ERRNO_DOA_PROC_BASE-4) |
Error Code: Out of HWA resources.
#define DPU_DOAPROC_ESEMA (DP_ERRNO_DOA_PROC_BASE-5) |
Error Code: Semaphore creation failed.
#define DPU_DOAPROC_ESEMASTATUS (DP_ERRNO_DOA_PROC_BASE-6) |
Error Code: Bad semaphore status.
#define DPU_DOAPROC_EEXCEEDHWAMEM (DP_ERRNO_DOA_PROC_BASE-7) |
Error Code: Configure parameters exceed HWA memory bank size.
#define DPU_DOAPROC_ECUBEFORMAT (DP_ERRNO_DOA_PROC_BASE-8) |
Error Code: Unsupported radar cube format.
#define DPU_DOAPROC_EDETMFORMAT (DP_ERRNO_DOA_PROC_BASE-9) |
Error Code: Unsupported detection matrix format.
#define DPU_DOAPROC_EDETMSIZE (DP_ERRNO_DOA_PROC_BASE-10) |
Error Code: Insufficient detection matrix size.
#define DPU_DOAPROC_EWINDSIZE (DP_ERRNO_DOA_PROC_BASE-11) |
Error Code: Wrong window size.
#define DPU_DOAPROC_E_NOTSUPPORTED_ANGLE_DIM_ONE_AND_CPU_LOOP_CTRL (DP_ERRNO_DOA_PROC_BASE-12) |
Error Code: Not supported angle dim 1 (no elevation) and.
#define DPU_DOAPROC_E_EXCEEDED_MAX_NUM_DOPPLER_BINS (DP_ERRNO_DOA_PROC_BASE-13) |
Error Code: Doppler FFT size exceeded the limit. Maximum Doppler index is stored in array of type uint8_t.