The section has a list of all the error codes which are generated by the module.
Base error code for the dpedma is defined in the
Macros | |
#define | DPEDMA_EINVAL (DP_ERRNO_DPEDMA_BASE-1) |
Error Code: Invalid argument. More... | |
#define | DPEDMA_EINVAL_EDMAADDR (DP_ERRNO_DPEDMA_BASE-2) |
Error Code: Invalid EDMA baseaddress. More... | |
#define | DPEDMA_EDMA_TRIGGER_FAIL (DP_ERRNO_DPEDMA_BASE-3) |
Error Code: EDMA transfer trigger failure. More... | |
#define DPEDMA_EINVAL (DP_ERRNO_DPEDMA_BASE-1) |
Error Code: Invalid argument.
#define DPEDMA_EINVAL_EDMAADDR (DP_ERRNO_DPEDMA_BASE-2) |
Error Code: Invalid EDMA baseaddress.
#define DPEDMA_EDMA_TRIGGER_FAIL (DP_ERRNO_DPEDMA_BASE-3) |
Error Code: EDMA transfer trigger failure.