ESM Driver API/interface file.
Go to the source code of this file.
Data Structures | |
struct | ESM_GroupIntrStatus |
Structure to access the status of interrupts belonging to a group. More... | |
struct | ESM_NotifyParams |
Parameters used to register the ESM notify function to handle Group1 and Group2 errors. The notify function will be invoked post the ESM FIQ interrupt handler processing. More... | |
struct | ESM_OpenParams |
ESM Open Parameters. More... | |
struct | ESM_Attrs |
ESM Hardware Atrributes. More... | |
struct | ESM_Object |
ESM Driver Object. More... | |
struct | ESM_Config |
ESM Instance configuration. More... | |
Macros | |
#define | ESM_ERRNO_BASE (-3000) |
ESM driver error base. More... | |
#define | ESM_EINVAL (ESM_ERRNO_BASE-1) |
Error Code: Invalid argument More... | |
#define | ESM_ENOINIT (ESM_ERRNO_BASE-2) |
Error Code: Operation cannot be done as ESM_open is not done. More... | |
#define | ESM_EREINIT (ESM_ERRNO_BASE-3) |
Error Code: Operation cannot be done as ESM_open is already done and re-init is not permitted. More... | |
#define | ESM_ENOMEM (ESM_ERRNO_BASE-4) |
Error Code: Out of memory. More... | |
#define | ESM_MAX_NOTIFIERS (4U) |
Maximum number of notify callbacks supported. More... | |
#define | ESM_MAX_ISR_COUNT (4U) |
Maximum ISR supported. More... | |
#define | CSL_APP_ESM_ESMEKR_EKEY_NORMAL_MODE (0x0U) |
#define | CSL_APP_ESM_ESMEKR_EKEY_ERROR_PIN_RESET (0x5U) |
#define | CSL_APP_ESM_ESMEKR_EKEY_ERROR_FORCE_MODE (0xAU) |
Typedefs | |
typedef void * | ESM_Handle |
A handle that is returned from a ESM_open() call. More... | |
typedef void(* | ESM_CallBack) (void *arg) |
Callback function which is invoked by the ESM module if a notify function is registered using the ESM_registerNotifier() API. More... | |
Enumerations | |
enum | ESM_IntrPriorityLvl { ESM_INTR_PRIORITY_LEVEL_LOW = 0x0U, ESM_INTR_PRIORITY_LEVEL_HIGH = 0x1U } |
Enum to select level for interrupt. More... | |
enum | ESM_OperationMode { ESM_OPERATION_MODE_NORMAL = CSL_APP_ESM_ESMEKR_EKEY_NORMAL_MODE, ESM_OPERATION_MODE_ERROR_FORCE = CSL_APP_ESM_ESMEKR_EKEY_ERROR_FORCE_MODE } |
Enum to select the ESM Operation Mode. More... | |
Functions | |
void | ESM_init (void) |
The functions initializes the ESM module. More... | |
void | ESM_deinit (void) |
The functions de-initializes the ESM module. More... | |
ESM_Handle | ESM_open (uint32_t index, ESM_OpenParams *params) |
Opens a ESM object with the index and parameters specified, and returns a ESM_Handle. More... | |
void | ESM_close (ESM_Handle handle) |
The function closes a ESM peripheral specified by the ESM handle. More... | |
int32_t | ESM_registerNotifier (ESM_Handle handle, ESM_NotifyParams *params, int32_t *errCode) |
Register the notifers. The ESM module will call back if error interrupt is detected. More... | |
int32_t | ESM_deregisterNotifier (ESM_Handle handle, int32_t notifyIndex, int32_t *errCode) |
Deregister the ESM notifers. More... | |
void | ESM_setMode (uint32_t baseAddr, uint32_t mode) |
This API is used to configure operation mode of ESM module. More... | |
int32_t | ESM_setErrPinLowTimePreload (uint32_t baseAddr, uint32_t lowTime) |
This API is used to configure the low time counter pre-load value. More... | |
uint32_t | ESM_getCurrErrPinLowTimeCnt (uint32_t baseAddr) |
This API is used to get the current value of low time counter. More... | |
uint32_t | ESM_getErrPinStatus (uint32_t baseAddr) |
This API is used to get the current status of nERROR pin. More... | |
void | ESM_resetErrPin (uint32_t baseAddr) |
This API is used to reset the nERROR pin. This will set the nERROR pin to high. More... | |
uint32_t | ESM_getIntrStatus (uint32_t baseAddr, uint32_t intrSrc) |
This API is used to get the interrupt status. More... | |
int32_t | ESM_getGroupIntrStatus (uint32_t baseAddr, uint32_t grpNum, ESM_GroupIntrStatus *intrstatus) |
This API is used to get the interrupt/error status for a group. More... | |
static void | ESM_Params_init (ESM_OpenParams *openPrms) |
Variables | |
ESM_Config | gEsmConfig [] |
Externally defined driver configuration array. More... | |
uint32_t | gEsmConfigNum |
Externally defined driver configuration array size. More... | |