Macros | |
#define | ESM_EINVAL (ESM_ERRNO_BASE-1) |
Error Code: Invalid argument More... | |
#define | ESM_ENOINIT (ESM_ERRNO_BASE-2) |
Error Code: Operation cannot be done as ESM_open is not done. More... | |
#define | ESM_EREINIT (ESM_ERRNO_BASE-3) |
Error Code: Operation cannot be done as ESM_open is already done and re-init is not permitted. More... | |
#define | ESM_ENOMEM (ESM_ERRNO_BASE-4) |
Error Code: Out of memory. More... | |
#define ESM_EINVAL (ESM_ERRNO_BASE-1) |
Error Code: Invalid argument
#define ESM_ENOINIT (ESM_ERRNO_BASE-2) |
Error Code: Operation cannot be done as ESM_open is not done.
#define ESM_EREINIT (ESM_ERRNO_BASE-3) |
Error Code: Operation cannot be done as ESM_open is already done and re-init is not permitted.
#define ESM_ENOMEM (ESM_ERRNO_BASE-4) |
Error Code: Out of memory.