xWRL1432 MMWAVE-L-SDK  05.03.00

Detailed Description

UART driver object.

Data Fields

UART_Handle handle
 
UART_Params prms
 
const void * writeBuf
 
uint32_t writeCount
 
uint32_t writeSizeRemaining
 
void * readBuf
 
uint32_t readCount
 
uint32_t readSizeRemaining
 
uint32_t rxTimeoutCnt
 
uint32_t readErrorCnt
 
UART_TransactionreadTrans
 
UART_TransactionwriteTrans
 
uint32_t isOpen
 
void * lock
 
SemaphoreP_Object lockObj
 
void * readTransferSem
 
SemaphoreP_Object readTransferSemObj
 
void * writeTransferSem
 
SemaphoreP_Object writeTransferSemObj
 
void * hwiHandle
 
HwiP_Object hwiObj
 
UART_EdmaParams rxEdmaParams
 
UART_EdmaParams txEdmaParams
 
EDMA_Handle uartEdmaHandle
 
CSL_app_uartRegs * pSCIRegs
 
uint8_t shiftJustification
 

Field Documentation

◆ handle

UART_Handle UART_Object::handle

Instance handle to which this object belongs

◆ prms

UART_Params UART_Object::prms

Open parameter as provided by user

◆ writeBuf

const void* UART_Object::writeBuf

Buffer data pointer

◆ writeCount

uint32_t UART_Object::writeCount

Number of Chars sent

◆ writeSizeRemaining

uint32_t UART_Object::writeSizeRemaining

Chars remaining in buffer

◆ readBuf

void* UART_Object::readBuf

Buffer data pointer

◆ readCount

uint32_t UART_Object::readCount

Number of Chars read

◆ readSizeRemaining

uint32_t UART_Object::readSizeRemaining

Chars remaining in buffer

◆ rxTimeoutCnt

uint32_t UART_Object::rxTimeoutCnt

Receive timeout error count

◆ readErrorCnt

uint32_t UART_Object::readErrorCnt

Line status error count

◆ readTrans

UART_Transaction* UART_Object::readTrans

Pointer to the current read transaction

◆ writeTrans

UART_Transaction* UART_Object::writeTrans

Pointer to the current write transaction

◆ isOpen

uint32_t UART_Object::isOpen

Flag to indicate whether the instance is opened already

◆ lock

void* UART_Object::lock

Instance lock - to protect across transfers

◆ lockObj

SemaphoreP_Object UART_Object::lockObj

Driver lock object

◆ readTransferSem

void* UART_Object::readTransferSem

Read Transfer Sync Sempahore - to sync between transfer completion ISR and task

◆ readTransferSemObj

SemaphoreP_Object UART_Object::readTransferSemObj

Read Transfer Sync Sempahore object

◆ writeTransferSem

void* UART_Object::writeTransferSem

Write Transfer Sync Sempahore - to sync between transfer completion ISR and task

◆ writeTransferSemObj

SemaphoreP_Object UART_Object::writeTransferSemObj

Write Transfer Sync Sempahore object

◆ hwiHandle

void* UART_Object::hwiHandle

Interrupt handle for controller ISR

◆ hwiObj

HwiP_Object UART_Object::hwiObj

Interrupt object

◆ rxEdmaParams

UART_EdmaParams UART_Object::rxEdmaParams

EDMA parameters for the UART Rx

◆ txEdmaParams

UART_EdmaParams UART_Object::txEdmaParams

EDMA parameters for the UART Tx

◆ uartEdmaHandle

EDMA_Handle UART_Object::uartEdmaHandle

◆ pSCIRegs

CSL_app_uartRegs* UART_Object::pSCIRegs

Pointer to register overlay

◆ shiftJustification

uint8_t UART_Object::shiftJustification

This is the number of bits the read data needs to be shifted. This is calculated using the data length. When data of fewer than eight bits in length is received, it is left-justified in SCIRD and padded with trailing zeros. Data read from the SCIRD should be shifted by software to make the received data rightjustified.