4.3. Release notes - 08_01_00¶
4.3.1. Features¶
Note
New features vs previous release are marked in bold.
4.3.1.1. Hardware support¶
AM65xx EVM and IDK with SR2 / SR2.1 support
4.3.1.2. Software features¶
Important
Below is a summary of key features. Refer individual SDK Components release notes for more details
4.3.1.2.1. Platform Development Kit (PDK)¶
RTOS device drivers running on R5F, A53
Supported drivers and modules
Board diagnostic library
CPSW2G, CPTS, SGMII/QSGMII, LWIP
CSL-FL (Chip support library)
GPIO
I2C
IPC (inter processor communication)
McASP
MMCSD with FATFS
OSAL
SBL secondary bootloader
SCI Client (DMSC interface)
SPI driver (SPI, QSPI, OSPI, Hyperflash)
UART
UDMA and DRU
CAL
DSS
enet (R5F)
FreeRTOS Support on R5
New Features
ID |
Description |
Module |
---|---|---|
PDK-9714 |
FreeRTOS ROV Support |
PDK Debug |
ETHFW-1699 |
Time-aware shaper (TAS) support for ICSSG |
PDK/ENET Driver |
ETHFW-1714 |
10-Mbps full-duplex support |
PDK/ENET Driver |
Note
pdk/emac driver was deprecated in 8.0 release. Please switch to use enet lld
i.e. The pdk/packages/ti/drv/emac has been replaced with pdk/packages/ti/drv/enet
pdk/packages/ti/drv/enet is available now and supports ICSSG ports too
Please refer to the EMAC to Enet LLD migration guide for further details [LINK].
IPC3.x is deprecated for AM65X starting in SDK 7.0. SDK 6.3 was the last release with support for IPC3.x for AM65X. IPC LLD, included with PDK, is the only supported IPC stack for AM65X.
4.3.1.2.2. FreeRTOS¶
FreeRTOS for R5F
lwIP TCP/IP stack integration for R5F
4.3.1.2.3. Code Gen Tools (CGT)¶
TI LLVM (CLANG) Compiler, assembler, linker for R5F
GCC compiler for A53
4.3.2. Device Support and Validation Information¶
AM65xx SR2
AM65xx SR2.1, Check PDK FAQ - Supported Cores by example applications for details
4.3.3. Upgrade and Compatibility¶
4.3.3.1. TI Arm Clang C/C++ Compiler¶
This is the first release which includes TI Arm Clang Compiler (tiarmclang) for the R5F cores. Prior releases used the TI Arm Compiler (armcl). There are migration steps that may be necessary for existing code running on the R5F cores. The software delivered on R5F from TI has aleady been migrated accordingly. Please review the PDK release notes (LINK) for additional links and developer pages dedicated Clang migration.
4.3.3.2. TI-RTOS vs. FreeRTOS¶
FreeRTOS is the default OS for R5F libraries and binaries starting in 08.00.00 release. In 08.01.00 release, FreeRTOS is the default build and TI-RTOS (Sysbios) is no longer supported or packaged as part of the SDK. Please review the PDK release notes (LINK) for additional links and developer pages dedicated FreeRTOS migration.
4.3.3.3. NDK vs. LwIP¶
LwIP is the default network stack starting in 08.00.00 release. In 08.01.00 release, NDK is no longer supported or packaged as part of the SDK.
4.3.3.4. Industrial Protocols¶
Industrial Protocols are not packaged with this SDK. Please refer to Industrial Protocols section for more information.
4.3.4. Fixed Issues¶
Key issues addressed by componets are called out in the component release notes - Refer PDK Release notes for PDK issues LINK
4.3.5. Known Issues¶
Refer to individual SDK Components release notes for known issues in each component
4.3.6. Change Requests¶
ID |
Head Line |
Original Fix Version |
New Fix Version |
Components |
---|---|---|---|---|
JACINTOREQ-1602 |
ICSSG: Profinet TSN features Defer |
08.01.00 |
08.02.00 |
Industrial Protocols |
JACINTOREQ-1851 |
ICSSG: Profinet TSN features Defer |
08.01.00 |
08.02.00 |
Industrial Protocols |
JACINTOREQ-1852 |
ICSSG: PDK Board Diagnostics Descope from SDK |
08.01.00 |
DESCOPE |
PDK |