4.6. Release notes - 07_01_00¶
4.6.1. Features¶
Note
New features vs previous release are marked in bold
4.6.1.1. Hardware support¶
AM65xx EVM and IDK with SR2 support
4.6.1.2. Software features¶
Important
Below is a summary of key features. Refer individual SDK Components release notes for more details
4.6.1.2.1. Platform Development Kit (PDK)¶
RTOS device drivers running on R5F, A53
Supported drivers and modules
Board diagnostic library
CPSW2G, CPTS, SGMII/QSGMII
CSL-FL (Chip support library)
GPIO
I2C
IPC (inter processor communication)
McASP
MMCSD with FATFS (A53 with RTOS)
OSAL
SBL secondary bootloader
SCI Client (DMSC interface)
SPI driver (SPI, QSPI, OSPI, Hyperflash)
UART
UDMA and DRU
CAL
DSS
New Features
ID |
Description |
Module |
---|---|---|
PDK-4928 |
Support Firewall control layer for TISCI features |
SCICLIENT |
PDK-5593 |
Support use case of MPU/Linux and MCU/Baremetal |
IPC |
Note
IPC3.x is deprecated for AM65X starting in SDK 7.0. SDK 6.3 was the last release with support for IPC3.x for AM65X. IPC LLD, included with PDK, is the only supported IPC stack for AM65X.
4.6.1.2.2. TI-RTOS¶
SysBIOS for R5F
Network developer kit (NDK) on R5F
4.6.1.2.3. Code Gen Tools (CGT)¶
TI Compiler, assembler, linker for R5F
GCC compiler for A53
4.6.2. Device Support and Validation Information¶
AM65xx SR2
4.6.3. Upgrade and Compatibility¶
MCUSW was delivered as part of previous release, but it has been removed from this release as it is not supported.
Industrial Protocols are not packaged with this SDK. Please refer to Industrial Protocols section for more information.
4.6.4. Known Issues¶
Refer to individual SDK Components release notes for known issues in each component