6. How to GuidesΒΆ
- 6.1. Host
- 6.1.1. How to Build a Ubuntu Linux host under VMware
 - 6.1.2. Connect to an EVM via Telnet
 - 6.1.3. How to Setup a Samba Server
 - 6.1.4. Boot Sequence
 - 6.1.5. Moving Files to the Target System
 - 6.1.6. How to Flash Linux System from U-boot
 - 6.1.7. Customizing the SDK Splash Screen
 - 6.1.8. AM335x ICEv2 flash erase
 - 6.1.9. Ubuntu 14.04 Set Up to Network Boot an AM335x/AM437x Based Platform
 - 6.1.10. How to Develop with 3D Graphics
 - 6.1.11. How to Develop accelerated Multimedia using GStreamer on AM57xx
 - 6.1.12. Preventing BeagleBone board reset on JTAG Connect
 - 6.1.13. Processor SDK IPC Quick Start Guide
 - 6.1.14. Create DSP and IPU firmware using PDK drivers and IPC to load from ARM Linux
 
 - 6.2. Target
- 6.2.1. How to Recalibrate the Touchscreen
 - 6.2.2. SDK File System Optimization/Customization
 - 6.2.3. How to add a JVM
 - 6.2.4. How to use a Mouse instead of the Touchscreen with Matrix
 - 6.2.5. Update U-Boot Environment Variables stored in SPI Flash from Linux
 - 6.2.6. How to change dtb files
 - 6.2.7. How to Boot Beagle Bone Black with Processor SDK Linux
 
 - 6.3. Hardware EVM Setup
 - 6.4. Board Port