Processor SDK Linux for AM65X
09_01_00_01
1. Overview
2. Release Specific
3. Foundational Components
4. Industrial Protocols
5. How to Guides
5.1. Developer Notes
5.1.1. Connect to an EVM via Telnet
5.1.2. How to Setup a Samba Server
5.1.3. Boot Sequence
5.1.4. Moving Files to the Target System
5.1.5. How to Flash from U-boot Shell
5.1.6. SDK File System Optimization/Customization
5.1.7. How to add a JVM
5.1.8. How to use a Mouse instead of the Touchscreen with Matrix
5.1.9. Update U-Boot Environment Variables stored in SPI Flash from Linux
5.1.10. How to change dtb files
5.1.11. How to Use K3Conf Tool
5.1.12. How do I integrate a different version of open source software than what is packaged in Processor SDK Linux AM65xx?
5.1.13. How to Build a Ubuntu Linux host under VMware
5.1.14. K3 Resource Partitioning Tool
5.2. Hardware EVM Setup
6. Documentation Tarball
Processor SDK Linux for AM65X
Docs
»
5.
How to Guides
»
5.1.
Developer Notes
»
5.1.3.
Boot Sequence
5.1.3.
Boot Sequence
ΒΆ