Processor SDK Linux for AM65X Logo
11_02_05_02
  • 1. Overview
  • 2. Release Specific
  • 3. Foundational Components
  • 4. Industrial Protocols
  • 5. Demo Applications
  • 6. How to Guides
    • 6.1. Developer Notes
      • 6.1.1. Moving Files to the Target System
      • 6.1.2. SDK File System Optimization/Customization
      • 6.1.3. How to add a JVM
      • 6.1.4. Update U-Boot Environment Variables stored in SPI Flash from Linux
      • 6.1.5. How to Use K3Conf Tool
      • 6.1.6. Real-Time Linux on TI SoCs
      • 6.1.7. How do I integrate a different version of open source software than what is packaged in Processor SDK Linux AM65xx?
      • 6.1.8. K3 resource partitioning tool
    • 6.2. Hardware EVM Setup
  • 7. Documentation Tarball
Processor SDK Linux for AM65X
  • 6. How to Guides
  • 6.1. Developer Notes
  • Edit on GitHub

6.1. Developer Notes

  • 6.1.1. Moving Files to the Target System
  • 6.1.2. SDK File System Optimization/Customization
    • 6.1.2.1. The Basics of OPKG
      • 6.1.2.1.1. List all available options of opkg
      • 6.1.2.1.2. Show all installed packages
      • 6.1.2.1.3. Show package contents
      • 6.1.2.1.4. Find a file owner
      • 6.1.2.1.5. Show packages which require the package as dependency
      • 6.1.2.1.6. Removing Packages or Deinstallation
      • 6.1.2.1.7. Install local packages
  • 6.1.3. How to add a JVM
  • 6.1.4. Update U-Boot Environment Variables stored in SPI Flash from Linux
  • 6.1.5. How to Use K3Conf Tool
    • 6.1.5.1. Overview
    • 6.1.5.2. How to use
  • 6.1.6. Real-Time Linux on TI SoCs
    • 6.1.6.1. What Is The Real-Time Linux Kernel?
    • 6.1.6.2. Validating We Are Using A Real-Time Capable Kernel
    • 6.1.6.3. Testing Kernel Performance
      • 6.1.6.3.1. Timer Based Applications
      • 6.1.6.3.2. Driver (Ethernet) Based Interrupts
    • 6.1.6.4. Tips For Tuning The Real-Time Kernel
      • 6.1.6.4.1. Technique to Tuning (Slow is Fast)
      • 6.1.6.4.2. Technique to Testing
      • 6.1.6.4.3. Disable Unnecessary Applications
      • 6.1.6.4.4. Disable Unnecessary Drivers
    • 6.1.6.5. Wrapping Up
  • 6.1.7. How do I integrate a different version of open source software than what is packaged in Processor SDK Linux AM65xx?
  • 6.1.8. K3 resource partitioning tool
Previous Next

© Copyright 1995-2026 Texas Instruments Incorporated, CC-BY-SA-4.0. Revision 537a93bc. Last updated on Jun 18, 2026.