6. How to Guides
- 6.1. Developer Notes
- 6.1.1. Moving Files to the Target System
- 6.1.2. SDK File System Optimization/Customization
- 6.1.3. How to add a JVM
- 6.1.4. Update U-Boot Environment Variables stored in SPI Flash from Linux
- 6.1.5. How to Use K3Conf Tool
- 6.1.6. Real-Time Linux on TI SoCs
- 6.1.7. How do I integrate a different version of open source software than what is packaged in Processor SDK Linux AM65xx?
- 6.1.8. K3 resource partitioning tool
- 6.2. Hardware EVM Setup