3.1.1.1. Setup
3.1.1.1.1. Install host dependencies
To install host dependencies for building TI U-boot source (standalone) on Ubuntu 22.04+, run the following command in the terminal prompt:
sudo apt install git xz-utils build-essential autoconf flex bison libssl-dev bc libncurses-dev \
python3 python3-setuptools python3-dev python3-yaml python3-jsonschema python3-pyelftools \
swig yamllint libgnutls28-dev
Note
The recommended host machine for building U-Boot is Ubuntu 22.04. Users of Ubuntu 18.04 might need to install Python 3.7 or later. If using the default Python 3.6 that is in Ubuntu 18.04, users might need to install these additional dependencies:
pip install dataclasses pyelftools jsonschema yamllint importlib-resources
3.1.1.1.2. Getting the Source Code
The easiest way to get access to the source code is by
downloading and installing the Processor SDK Linux. Once installed,
the source code is in the SDK at the path <path to tisdk>/board-support.
For your convenience the sources also includes
git repositories including commit history.
U-Boot sources can also be directly fetched from GIT. The GIT repository URL, branch and commit id is available in Build Information.