3.6.3.4. PRU_ICSSG Two Port Ethernet Switch¶
PRU_ICSSG can operate as VLAN aware Switch mode with two external physical ports and one internal host port. By default, interfaces come up in Dual independent EMAC mode and can be changed to operate in Switch mode at runtime. Note that changing from Dual EMAC to Switch mode needs loading of different firmwares to various PRU cores and thus have to follow specific sequence as shown in below sections:
3.6.3.4.1. Enabling Switch mode¶
Example assuming ETH1 and ETH2 as ICSSG0 interfaces:
ip link set dev eth1 down
ip link set dev eth2 down
devlink dev param set platform/icssg0-eth name switch_mode value 1 cmode runtime
ip link add name br0 type bridge
ip link set dev eth1 master br0
ip link set dev eth2 master br0
ip link set dev br0 up
ip link set dev eth1 up
ip link set dev eth2 up
bridge vlan add dev br0 vid 1 pvid untagged self
3.6.3.4.2. Going back to Dual EMAC mode¶
ip link set dev br0 down
ip link set dev eth1 nomaster
ip link set dev eth2 nomaster
ip link set dev eth1 down
ip link set dev eth2 down
devlink dev param set platform/icssg0-eth name switch_mode value 0 cmode runtime
ip link del name br0 type bridge
ip link set dev eth1 up
ip link set dev eth2 up
3.6.3.4.3. Turn On/Off Spanning Tree Protocol (STP)¶
ip link set dev br0 type bridge stp_state 1/0
3.6.3.4.4. VLAN configuration¶
bridge vlan add dev br0 vid 1 pvid untagged self <---- add cpu port to VLAN 1
This step is mandatory for bridge/default_pvid.
3.6.3.4.5. Adding extra VLANs¶
untagged:
bridge vlan add dev eth1 vid 100 pvid untagged master bridge vlan add dev eth1 vid 100 pvid untagged master bridge vlan add dev br0 vid 100 pvid untagged self <---- Add cpu port to VLAN100tagged:
bridge vlan add dev eth1 vid 100 master bridge vlan add dev eth1 vid 100 master bridge vlan add dev br0 vid 100 pvid tagged self <---- Add cpu port to VLAN100
3.6.3.4.6. Forwarding Data Bases (FDBs)¶
Forwarding entries for MAC addresses are automatically added on the appropriate switch port upon detection as default operation as an unmanaged bridge. For managed bridge operation manually add FDB entries as required.
Manually adding FDBs:
bridge fdb add aa:bb:cc:dd:ee:ff dev eth1 master vlan 100
bridge fdb add aa:bb:cc:dd:ee:fe dev eth1 master <---- Add on all VLANs
3.6.3.4.7. Multicast Data Bases (MDBs)¶
Multicast entries are automatically added on the appropriate switch port upon detection as default operation as an unmanaged bridge. For managed bridge operation manually add MDB entries as required.
Manually adding MDBs:
bridge mdb add dev br0 port eth1 grp 239.1.1.1 permanent vid 100
bridge mdb add dev br0 port eth1 grp 239.1.1.1 permanent <---- Add on all VLANs
3.6.3.4.8. Multicast flooding¶
CPU port mcast_flooding is always on
Turning flooding on/off on switch ports:
bridge link set dev eth1 mcast_flood on/off
3.6.3.4.9. Limitations of switch mode offloading support¶
- VLAN offloading is limited to 0-256 VIDs.
- MDB/FDB static entries are limited to 511 entries and different FDBs can hash to same bucket and thus may not be completely offloaded
3.6.3.4.10. SRAM Requirement¶
- The ICSSG Ethernet driver can be used in switch mode. Two icssg ports are used per switch.
- SRAM Required for each switch (per two ports) is 256 KB.
- For each ICSSG switch, the SRAM required needs to be contiguous.
- PRUETH only uses the required amount of SRAM from the SRAM/MSMC pool. If PRUETH doesn’t get the required amount of SRAM, the prueth_probe() API will return with -ENOMEM error.