6.1. Developer NotesΒΆ
- 6.1.1. Connect to an EVM via Telnet
- 6.1.2. How to Setup a Samba Server
- 6.1.3. Moving Files to the Target System
- 6.1.4. SDK File System Optimization/Customization
- 6.1.5. MCAN on AM62x
- 6.1.6. How to enable DT overlays in linux
- 6.1.7. How to playback audio over HDMI
- 6.1.8. How to configure K3 MSMC memory for use as SRAM or L3 cache?
- 6.1.9. How to check some device tree information from user-space of Linux?
- 6.1.10. How do I integrate a different version of open source software than what is packaged in Processor SDK Linux AM62Ax?
- 6.1.11. How to Build a Ubuntu Linux host under VMware
- 6.1.12. K3 Resource Partitioning Tool
- 6.1.13. SYSFW Trace Parser