6.1.2. How to Setup a Samba Server¶
Introduction
When using a Virtual machine you may share files & folders via the Share Foldr feature of that partoicular Virtual Machine. Another alternative, especially if you are using a dedicated Linux host, is to configure a Samba server on your Linux host.
Samba allows a host to interact with a Microsoft Windows client or server as if it is a Windows file and print server. In other words, if you are installing software on a Windows machine, you can easily transfer/modify files to the host machine by accessing it (the host machine) through windows.
Installing a Samba Server
1. Samba can be installed by opening a terminal. (Applications -> System Tools -> Terminal)
2. Switch to root user by typing su and entering the password you set during the install.
- On Fedora install Samba with the yum command: system-config-samba
- Open the Samba GUI (System -> Administration -> Samba).
- Configure the share
![../../../_images/Samba_Server_Configuration_001.png](../../../_images/Samba_Server_Configuration_001.png)
- Click on “Add Share”
- Specify the directory you want to share. For example, /home/<username>
![../../../_images/Create_Samba_Share_002.png](../../../_images/Create_Samba_Share_002.png)
- Check both the Writable and Visable boxes
- On the “Access” tab, select the Allow access to everyone option
![../../../_images/Create_Samba_Share_003.png](../../../_images/Create_Samba_Share_003.png)
- Select “OK”
- Set up the workgroup
- From the toolbar, select Preferences -> Server Settings
![../../../_images/Server_Settings_004.png](../../../_images/Server_Settings_004.png)
- Specify the “Workgroup” to match the workgroup on your Windows environment
- Select “OK”
- Add a user
- From the toolbar, select Preferences -> Samba Users
- Click “Add User”
- From the “Unix Username” dropdown box, select the username you set up
- In the “Windows Username” and password boxes, enter the Unix Username and password for that user, respectively.
- Select “OK”
- Turn off the firewall
- System -> Administration -> Firewall
- Select the “Disable” button
NOTE - If you are within your company’s firewall you may need to configure the network proxy.
- Enable the Samba and NFS services
- System -> Administration -> Services (NOTE - Not available in Ubuntu 10.04 LTS. However the Samba service should start automatically)
- Enable the services by browsing through the list on the left and locating nfs and smb. If they are not already enabled, enable them by clicking the “Enable” button.
- Test the configuration
- From a terminal on the Linux workstation, type the command <prompt> ifconfig and note the IP address
- From your Windows machine, go to Start -> Run and type \<IP_ADDR> replacing <IP_ADDR> with the IP address of the Linux system