5.1. HostΒΆ
- 5.1.1. How to Build a Ubuntu Linux host under VMware
- 5.1.2. Connect to an EVM via Telnet
- 5.1.3. How to Setup a Samba Server
- 5.1.4. Boot Sequence
- 5.1.5. Moving Files to the Target System
- 5.1.6. Customizing the SDK Splash Screen
- 5.1.7. How to Develop with 3D Graphics
- 5.1.8. Preventing BeagleBone board reset on JTAG Connect
- 5.1.9. Processor SDK IPC Quick Start Guide
- 5.1.10. Create DSP and IPU firmware using PDK drivers and IPC to load from ARM Linux