5. How to GuidesΒΆ
- 5.1. Host
- 5.1.1. How to Build a Ubuntu Linux host under VMware
- 5.1.2. Connect to an EVM via Telnet
- 5.1.3. How to Setup a Samba Server
- 5.1.4. Boot Sequence
- 5.1.5. Moving Files to the Target System
- 5.1.6. Customizing the SDK Splash Screen
- 5.1.7. How to Develop with 3D Graphics
- 5.1.8. Preventing BeagleBone board reset on JTAG Connect
- 5.1.9. Processor SDK IPC Quick Start Guide
- 5.1.10. Create DSP and IPU firmware using PDK drivers and IPC to load from ARM Linux
- 5.2. Target
- 5.2.1. How to Recalibrate the Touchscreen
- 5.2.2. SDK File System Optimization/Customization
- 5.2.3. How to use a Mouse instead of the Touchscreen with Matrix
- 5.2.4. Update U-Boot Environment Variables stored in SPI Flash from Linux
- 5.2.5. How to change dtb files
- 5.2.6. How to Set Display for AM572x GP EVM
- 5.3. Hardware EVM Setup
- 5.4. Linux Porting Guide for AM571x/AM570x Speed Grades