2.3. Yocto Layer ConfigurationΒΆ
Processor SDK uses the following oe-layersetup configs to configure the meta layers. These are the <config> used in the command:
$ ./oe-layertool-setup.sh -f <config>
The following config files are located in the configs/processor-sdk directory of the oe-layersetup git repo.
Config File |
Description |
Supported machines/platforms |
|---|---|---|
processor-sdk-09.01.00-legacy-config.txt |
Processor SDK 09.01.00.01 Release |
am335x-evm, am437x-evm |