2.1. Release Notes

2.1.1. Overview

The Processor Software Development Kit (Processor SDK) is a unified software platform for TI embedded processors providing easy setup and fast out-of-the-box access to benchmarks and demos. All releases of Processor SDK are consistent across TI’s broad portfolio, allowing developers to seamlessly reuse and develop software across devices. Developing a scalable platform solutions has never been easier than with the Processor SDK and TI’s embedded processor solutions.

To simplify the end user experience, Processor SDK Linux AM64x installer provides everything needed as discussed below to create the embedded system from “scratch” :

  • Platform/board-support software and configuration files for Linux

  • U-Boot and Kernel sources and configuration files

  • An ARM cross-compiling toolchain as well as other host binaries and components

  • A Yocto/OE compliant filesystem and sources for example applications

  • A variety of scripts and Makefiles to automate certain tasks

  • Other components needed to build an embedded system that don’t fit neatly into one of the above buckets

  • Reference Examples, benchmarks

This release supports SR2.0 High Security - Field Securable (HS-FS) devices. For migration guide and other info, refer GP to HS-FS Migration Guide

2.1.2. Licensing

Please refer to the software manifests, which outlines the licensing status for all packages included in this release. The manifest can be found on the SDK download page or in the installed directory as indicated below.

  • Linux Manifest: <PSDK_PATH>/manifest/software_manifest.htm

2.1.3. Release 11.01.05.03

Released on July 2025

2.1.3.1. What’s new

Processor SDK Linux AM64X Release has following new features:

  • Second 2025 LTS Reference Release Including RT combined branch model - Kernel: PRU HW UART - Important Bug Fixes on top of Processor SDK 11.00.09.04 Release - Review Issue Tracker Section for the new fixes.

  • This release adds support for PRP Offload to the ICSSG prueth-driver. This allows to offload PRP functionality to the ICSSG hardware, which helps in reducing load on the A53 cores.

Key Release References:

Component version:

  • Kernel 6.12.35

  • U-Boot 2025.01

  • Toolchain GCC 13.4

  • ATF 2.13+

  • OPTEE 4.6.0

  • TIFS Firmware v11.01.02 (Click on the link for more information)

  • Yocto scarthgap 5.0

2.1.4. Build Information

2.1.4.1. U-Boot

u-boot

Head Commit: d2a72467939e169210bcd8e57de4b3e6ce2ef149 TI: dts: arm64: ti: sync dtbs from ti-linux-6.12.y upto e3e551586dfa
uBoot Version: 2025.01
uBoot Description: RC Release 11.01.05
Clone: git://git.ti.com/ti-u-boot/ti-u-boot.git
Branch: ti-u-boot-2025.01
uBoot Tag: 11.01.05

2.1.4.2. TF-A

Head Commit: e0c4d3903b382bf34f552af53e6d955fae5283ab Merge changes from topic “xlnx_fix_gen_con_datatype” into integration
Branch: master
Tag: (2.13 based)

2.1.4.3. OP-TEE

Head Commit: 71785645fa6ce42db40dbf5a54e0eaedc4f61591 Update CHANGELOG for 4.6.0
Branch: master
Tag: 4.6.0

2.1.4.4. ti-linux-firmware

Head Commit: 33bec0e2ea9a25362c0c8243b2f1ed392dbc5b02 Merge branch ‘main’ of git://git.kernel.org/pub/scm/linux/kernel/git/firmware/linux-firmware into ti-linux-firmware-next
Branch: ti-linux-firmware
Tag: 11.01.05

2.1.4.5. Kernel

Linux Kernel

Head Commit: e3e551586dfad357550da433969d6d9f458e06ce PENDING: arm64: dts: ti: k3-am62d2: Enable heartbeat led
Kernel Version: v6.12.35
Kernel Description: RC Release 11.01.05
Repo: git://git.ti.com/ti-linux-kernel/ti-linux-kernel.git
Branch: ti-linux-6.12.y
Tag: 11.01.05
use-kernel-config=defconfig
non-rt-config-fragment=kernel/configs/ti_arm64_prune.config
rt-config-fragment=config-fragment=kernel/configs/ti_arm64_prune.config kernel/configs/ti_rt.config

2.1.4.6. Yocto

meta-ti

Head Commit: 59354be6c2362b9f7d0a3cd2c017f2f3c6ab7f2e CI/CD Auto-Merger: cicd.scarthgap.202507011953
Clone: git://git.yoctoproject.org/meta-ti
Branch: scarthgap
Release Tag: 11.01.05

meta-arago

Head Commit: 0a9d75bc9eab472baa1eef57e1166954c557550a CI/CD Auto-Merger: cicd.scarthgap.202506261626
Clone: git://git.yoctoproject.org/meta-arago
Branch: scarthgap
Release Tag: 11.01.05

meta-tisdk

Head Commit: 3265fc78d1dddd1642c112a2f3f42507bfa176d9 meta-ti-foundational: ti-apps-launcher: Update SRCREV
Branch: scarthgap
Release Tag: 11.01.05.03

2.1.5. Issues Tracker

Note

  • Release Specific Issues including details will be published through Software Incident Report (SIR) portal

  • Further Information can be found at SIR Portal <https://sir.ext.ti.com/>

2.1.5.1. Errata Resolved

Record ID

Title

EXT_EP-12122

USB2 PHY locks up due to short suspend

EXT_EP-12123

USART: Erroneous clear/trigger of timeout interrupt

EXT_EP-12114

MMCSD: HS200 and SDR104 Command Timeout Window Too Small

2.1.5.2. Issues Resolved

Record ID

Title

EXT_SITMPUSW-74

Resource Table generating wrong format for rm-cfg.yaml

EXT_EP-12816

SDK Docs: Broken URL in How To Guides > EVM Setup

EXT_EP-12820

AM64x UDP title missing from performance guide

EXT_EP-12748

AM64x CPSW UDP tests missing from Performance Guide

EXT_EP-12760

CPSW Multicast packets not received on one eth interface when other eth interface links up

EXT_EP-12781

AM64x Software Buildsheet: incorrect information

EXT_EP-12310

Resource Table generating wrong format for rm-cfg.yaml

EXT_EP-12285

SK-AM64B: Deferred probe of i2c bus warning

EXT_EP-12300

ICSSG: Ethernet: Promiscuous mode is always enabled in bridge mode

EXT_EP-12821

ethtool does not count PRU Ethernet TX frames

EXT_SITMPUSW-146

Yocto: meta-ti*: kernel source has uncommited changes

2.1.5.3. Issues Open

Record ID

Title

EXT_EP-12750

TMDS64EVM: PCIe refclk contention

EXT_EP-12819

AM64x CICD does not test PRU

EXT_EP-12818

PRU RPMsg swaps which message is sent to which core

EXT_EP-12075

U-boot gets stuck when DDR size changed to 512 MB

EXT_EP-12827

bridged traffic CPSW3G is not following VLAN priority for preemptable traffic

EXT_EP-12749

cdns: device mode: Linux hangs when USB cable is disconnected

EXT_EP-12060

AM64x: Lower core count on variant devices no supported

EXT_EP-12785

Cyclictest performance degradation on AM62x/AM64x/AM62A

EXT_EP-12815

UDP Ingress failing