3.1.2.8. Keywriter Lite

This OTP (One Time Programmable) keywriter lite guide describes the procedure to be followed to populate customer keys in eFuses of the SoC.

OTP Keywriter Lite is used to convert the HS-FS device to a HS-SE Lite device(without encryption support). It is used to program only public keys hash.

Caution

Once the SoC eFuses are programmed using keywriter lite, there is no going back. This action of burning the OTP fields is irreversible.

High Security (HS) Device Sub-types

HS-FS (High Security - Field Securable): Device type before customer keys are programmed (the state in which the device leaves TI factory). In this state, device protects the ROM code, TI keys and certain security peripherals. HS-FS devices do not enforce secure boot process.

HS-SE Lite (High Security - Security Enforced Lite): Device type after only the customer public key hashes are programmed. HS-SE Lite devices enforce secure boot (without encryption).

HS-FS to HS-SE Lite Conversion

In order to convert a HS-FS device to HS-SE Lite device, one has to program the customer root key (optionally backup key) on the target device, using OTP Keywriter Lite.

Customer key information is put in a structured format to create a binary blob (Uboot keywriter lite structure).

Uboot Keywriter Lite Structure

struct fuse_otp_header {
    uint32_t version_info;
    uint32_t fuse_mode;
} __attribute__((packed));

struct fuse_otp {
    struct fuse_otp_header fuse_otp_hdr;
    struct fuse_otp_blob fuse_otp_blb;
} __attribute__((packed));
  • version_info : Customer can use this field to denote the version of uboot fuse programming.

  • fuse_mode : Fuse mode with value 0x00009045.

The overall fuse_otp structure is shown below:

../../../_images/Uboot_fuse_writebuff_OTP_structure.png

Attention

For information on the fuse_otp_blob structure, visit keywriter_lite_cert_gen_procedure.

Generate the Binary Blob

Generate the binary blob based out of U-boot keywriter lite structure by populating the structure and extracting the .data section to a bin file and copy it to SD card.

Typical Keywriter Lite Flow

A typical flow to do OTP keywriter lite is as follows:

  1. Addr 0x82000000 is the dedicated address to store the generated keywriter lite binary blob. Clear out 1Kb of memory starting from 0x82000000:

    => mw 0x82000000 0 0x400
    
  2. The binary blob copied to SD card can be loaded into memory using commands like:

    => fatload mmc 1:1 0x82000000 keywriter_lite_blob.bin
    
  3. Read the memory address 0x82000000 to verify that you loaded the blob successfully.

    => md 0x82000000
    
  4. Efuse modification requires a voltage to be applied on a specific pin (Vpp) during the programming. To program the efuses, the Vpp pin on the System-on-Chip (SoC) must be powered at 1.8V. It is the responsibility of the SoC user to design a suitable circuit that enables the Vpp pin to be powered.

    Texas Instruments (TI) EVMs feature an I2C-based IO expander, which has one of its IO pins connected to the SoC’s Vpp pin. The software required to control the power to the Vpp pin depends on the specific circuit implementation.

    In the case of TI AM62L PROC181E1 EVMs, an I2C driver is necessary to send command packets to the IO expander, which then toggles the IO pin connected to the Vpp pin, thereby controlling the power supply to the pin. On TI EVM, Vpp pin can be turned on using the below commands:

    Select i2c bus 1, as chip 22 is connected to it, and probe the chip:

    => i2c dev 1
    => i2c probe 22
    

    To turn off Vpp:

    => i2c mw 0x22 0x04 0x00
    

    To configure Vpp (port 04) as output:

    => i2c mw 0x22 0xC 0xEF
    

    To turn on Vpp:

    => i2c mw 0x22 0x04 0x10
    
  5. Call fuse writebuff sub-system command with the address 0x82000000:

    => fuse writebuff -y 0x82000000
    
  6. Turn off Vpp after programming is successful:

    => i2c mw 0x22 0x04 0x00
    

Note

Changes made to efuses, by programming them, take effect (like become visible in Memory-Mapped Registers (MMRs), device type change etc.) after a complete System-on-Chip (SoC) power cycle.