3.1.2.9. Keywriter
This OTP (One Time Programmable) keywriter guide describes how to populate customer keys in eFuses of the SoC.
OTP Keywriter is used to convert the HS-FS device to a HS-SE device(with encryption support). It is used to program both public keys hash and symmetric keys.
Caution
Once you program the SoC eFuses using keywriter, there is no going back. This action of burning the OTP fields is irreversible.
High Security (HS) Device Sub-types
HS-FS (High Security - Field Securable): Device type before you program customer keys (the state in which the device leaves TI factory). In this state, device protects the ROM code, TI keys and certain security peripherals. HS-FS devices do not enforce secure boot process.
HS-SE (High Security - Security Enforced): Device type after you program the customer keys. HS-SE devices enforce secure boot (with encryption).
HS-FS to HS-SE Conversion
To convert a HS-FS device to HS-SE device, program the customer root key (optionally backup key) on the target device by using OTP Keywriter.
Customer key information is encrypted into a x509 certificate to create a binary blob.
U-Boot Keywriter Structure
struct fuse_otp_header {
uint32_t version_info;
uint32_t fuse_mode;
} __attribute__((packed));
struct fuse_otp {
struct fuse_otp_header fuse_otp_hdr;
struct fuse_otp_blob fuse_otp_blb;
} __attribute__((packed));
version_info : Customer can use this field to denote the version of U-Boot fuse programming.
fuse_mode : Fuse mode with value 0x00009031.
The following shows the overall fuse_otp structure:
Attention
For information about the fuse_otp_blob x509 keywriter certificate, visit keywriter_cert_gen_procedure.
Generate the Binary Blob
Generate the binary blob based out of U-Boot Keywriter x509 certificate and copy the bin file to a SD card.
Typical Keywriter Flow
A typical flow to do OTP keywriter is as follows:
Address 0x82000000 is the dedicated address to store the generated keywriter binary blob. Clear out 12Kb of memory starting from 0x82000000:
=> mw 0x82000000 0 0x3000
Load the binary blob from SD card into memory using commands such as:
=> fatload mmc 1:1 0x82000000 keywriter_blob.bin
Read the memory address 0x82000000 to verify that you loaded the blob successfully.
=> md 0x82000000
Efuse modification requires a voltage to be applied on a specific pin (Vpp) during the programming. To program the efuses, the Vpp pin on the System-on-Chip (SoC) must be powered at 1.8V. It is the responsibility of the SoC user to design a suitable circuit that enables the Vpp pin to be powered.
Texas Instruments (TI) EVMs feature an I2C-based IO expander, which has one of its IO pins connected to the SoC’s Vpp pin. The software required to control the power to the Vpp pin depends on the specific circuit implementation.
In the case of TI AM62L PROC181E1-1 EVMs, an I2C driver is necessary to send command packets to the IO expander, which then toggles the IO pin connected to the Vpp pin, thereby controlling the power supply to the pin. On TI EVM, turn on the Vpp pin using the following commands:
Select i2c bus 1, as chip 22 is connected to it, and probe the chip:
=> i2c dev 1 => i2c probe 22
To turn off Vpp:
=> i2c mw 0x22 0x04 0x00
To configure Vpp (port 04) as output:
=> i2c mw 0x22 0xC 0xEF
To turn on Vpp:
=> i2c mw 0x22 0x04 0x10
Call fuse writebuff sub-system command with the address 0x82000000:
=> fuse writebuff -y 0x82000000
Turn off Vpp after programming is successful:
=> i2c mw 0x22 0x04 0x00
Note
Changes made to efuses, by programming them, take effect (such as becoming visible in Memory-Mapped Registers (MMRs), device type change and so on) after a complete System-on-Chip (SoC) power cycle.