2.5.1. RT-linux 11.01 Performance Guide
Read This First
All performance numbers provided in this document are gathered using following Evaluation Modules unless otherwise specified.
Name |
Description |
|---|---|
AM62Ax SK |
AM62Ax Starter Kit with ARM running at 1.2GHz, DDR data rate 3733 MT/S |
Table: Evaluation Modules
About This Manual
This document provides performance data for each of the device drivers which are part of the Processor SDK Linux package. This document should be used in conjunction with release notes and user guides provided with the Processor SDK Linux package for information on specific issues present with drivers included in a particular release.
If You Need Assistance
For further information or to report any problems, contact https://e2e.ti.com/ or https://support.ti.com/
2.5.1.1. System Benchmarks
Stress-ng and Cyclic Test
stress-ng (next-generation) will stress test a embedded platform in various selectable ways. It was designed to exercise various physical subsystems as well as the various operating system kernel interfaces. stress-ng can also measure test throughput rates; this can be useful to observe performance changes across different operating system or types of hardware.
Cyclictest is most commonly used for benchmarking RT systems. It is one of the most frequently used tools for evaluating the relative performance of real-time systems. Some performance tests which use Cyclictest are System benchmarking, Latency debugging with tracing and approximating application performance.
Test commands used for running stress-ng and cyclictest together
stress-ng --cpu-method=all -c 4 &
cyclictest -m -Sp80 -D6h -h400 -i200 -M -q
The following summarizes the latencies observed using the yocto based default SDK image:
Note
A known issue in this SDK release is affecting this benchmark. Using OP-TEEs PRNG drivers rather than the hardware accelerated TRNG drivers restores the context switch latencies to the values you see here.
More information on switching to the PRNG drivers can be found in the Foundational Components section, here Building OP-TEE with Pseudo RNG drivers
Latencies |
CPU 0 |
CPU 1 |
CPU 2 |
CPU 3 |
|---|---|---|---|---|
Minimum (us) |
5 |
5 |
5 |
5 |
Average (us) |
6 |
6 |
6 |
6 |
Maximum (us) |
31 |
29 |
30 |
30 |