2.2. Software Build Sheet

Build Sheet of supported features and modules for this Processor SDK Linux AM62Ax Release. The following table lists the supported features and modules with the support status for Linux on A53. Please refer to RTOS Build Sheet for the supported features and modules on RTOS.

The support status is indicated by the following codes:

  • “Yes”: The feature or module is supported.

  • “No”: The feature or module is not supported.

  • “SDKx.y”: The feature or module will be supported in a future version of the SDK.

  • “NA”: The feature or module is not applicable in the hardware.

  • “ANY”: The feature or module is a new update in this revision of the SDK.

Table 2.1 Software Build Sheet

Category

Module

SubModule

Linux on A53

System Interconnect

Bandwidth regulator

No

CBASS auto-clock gating

No

Initialization

I2C Bootloader Operation

No

SPI Bootloader Operation

No

QSPI Bootloader Operation

NOR

No

NAND

No

OSPI Bootloader Operation

NOR

Yes

NAND (1-bit mode)

Yes

NAND (8-bit mode)

Yes

GPMC Bootloader Operation

NOR

No

NAND

Yes

Ethernet Bootloader Operation

Yes

USB Bootloader Operation

Host

No

Device

Yes

MMCSD Bootloader Operation

SD Card (no UHS)

Yes

eMMC

Yes

UART Bootloader Operation

Yes

Device Configuration

Power Supply Modules

POK

No

POR

No

PRG

No

PGD

No

VTM

Yes

Power MaNAgement

Deep Sleep Low Power Mode

Yes

Deep Sleep LPM Wakeup Events

RTC Timer

Yes

GT Timers

No

WKUP UART

Yes

I2C

No

MCU GPIO

Yes

I/O Daisy Chain

Yes

USB Connect/Disconnect

Yes

USB Remote Wakeup

Yes

MCU-Only Low Power Mode

Yes

Standby Low Power Mode

SDK11.1

Partial I/O Low Power Mode

Yes

IO + DDR low power mode

Yes

Boot-time OPP configurations

Yes

Runtime Power MaNAgement

Yes

DFS/CPUFreq

Yes

CPUIdle (A53 WFI)

Yes

CPUIdle (DDR in Self-Refresh)

No

Interprocessor Communication

Mailbox

Yes

Spinlock

Yes

Memory Controllers

DDR Subsystem (DDRSS)

DDR4

Yes

LPDDR4

Yes

Inline ECC (1bit err)

Yes

Inline ECC (mbit err)

No

Region-based Address Translation

No

Time Sync

Time Sync Module (CPTS)

Yes

Timer MaNAger

No

Time Sync and Compare Events

No

Data Movement Architecture (DMA)

Data Movement Subsystem (DMSS)

Yes

Peripheral DMA (PDMA)

Yes

RingAcc

Yes

BCDMA

Yes

Packet Streaming Interface Link

Yes

General Connectivity Peripherals

Multichannel Audio Serial Port (McASP)

Input

Yes

(MAIN domain)

Output

Yes

HDMI Output

Yes

General-Purpose Interface (GPIO)

Yes

Inter-Integrated Circuit (I2C)

Controller

Yes

Target

No

Multichannel Serial Peripheral Interface (McSPI)

Controller

Yes

Peripheral

No

Universal Asynchronous Receiver/Transmitter (UART)

UART

Yes

RS-485

Yes

IrDA

No

General Connectivity Peripherals

General-Purpose Interface (GPIO)

Yes

(MCU domain)

Inter-Integrated Circuit (I2C)

Controller

Yes

Target

No

Multichannel Serial Peripheral Interface (McSPI)

Controller

Yes

Peripheral

No

Universal Asynchronous Receiver/Transmitter (UART)

UART

Yes

RS-485

Yes

IrDA

No

General Connectivity Peripherals

Inter-Integrated Circuit (I2C)

Controller

Yes

(WKUP domain)

Target

No

Universal Asynchronous Receiver/Transmitter (UART)

UART

Yes

RS-485

Yes

IrDA

No

High-speed Serial Interfaces

Gigabit Ethernet Switch (CPSW3G)

Switch

Yes

EndPoint

Yes

TSN

Yes

TSN - VLAN

Yes

Universal Serial Bus Subsystem (USBSS)

Host 3.1

NA

Device 3.1

NA

Host 2.0

Yes

Device 2.0

Yes

Memory Interfaces

Flash Subsystem (FSS)

No

Quad Serial Peripheral Interface (QSPI)

NOR

No

NAND

NA

Octal Serial Peripheral Interface (OSPI)

NOR

Yes

NAND

Yes

Expanded Serial Peripheral Interface (xSPI)

Yes

General-Purpose Memory Controller (GPMC)

FPGA

NA

NAND

Yes

NOR

No

etc.

No

Error Location Module (ELM)

Yes

Multimedia Card Secure Digital (MMCSD) Interface

SD Card

Yes

eMMC

Yes

Industrial & Control Interfaces

Controller Area Network (MCAN) - MAIN domain

CAN

Yes

CAN FD

Yes

Controller Area Network (MCAN) - MCU domain

CAN

No

CAN FD

No

Enhanced Capture (ECAP) Module

Capture

Yes

PWM

Yes

Enhanced Pulse Width Modulation (EPWM) Module

Yes

Enhanced Quadrature Encoder Pulse (EQEP) Module

No

Camera Subsystem

Camera Streaming Interface Receiver (CSI_RX_IF)

Yes

MIPI D-PHY Receiver (DPHY_RX)

Yes

Multiple Camera

Yes

OV2312 RGB + IR sensor

Yes

iMX219 sensor

Yes

Timer Modules

Global Timebase Cunter (GTC)

Yes

Windowed Watchdog Timer (WWDT) - MAIN domain

Yes

Windowed Watchdog Timer (WWDT) - MCU domain

NA

Windowed Watchdog Timer (WWDT) - WKUP domain

NA

Real-Time Clock (RTC)

Yes

Timers - MAIN domain

Timer

Yes

Capture

No

Compare

No

PWM

Yes

Timers - MCU domain

Timer

No

Capture

No

Compare

No

PWM

No

Timers - WKUP domain

Timer

Yes

Capture

No

Compare

No

PWM

No

Internal Diagnostics Modules

Dual Clock Comparator (DCC)

No

Error Signalling Module (ESM)

No

Memory Cyclic Redundancy Check (MCRC) Controller

Yes

SDL Driver Porting Layer(SDL DPL)

No

RTI(WWDG)

No

Voltage and Thermal Management(VTM)

No

Interconnect Isolation Gasket(STOG)

No

Interconnect Isolation Gasket(MTOG)

No

Power OK(POK)

No

PBIST(Built In Self Test)

No

ECC Aggregator

No

DISPLAY Subsystem

Open LVDS Display Interface Transmitter (OLDITX)

NA

DISPLAY Parallel Interface (DPI)

Yes

Dual Display

NA

Video Processing Unit

Yes

Image Encoder

JPEG Encoder E5010

Yes

On-Die Temperature sensor

Yes

On-Chip Debug

Yes

Crypto Accelerator (SA3UL)

Advanced Encryption Standard (AES)

AES-CBC

Yes

AES-ECB

Yes

SHA/MD5 Crypto Hardware-Accelerated Module (SHA/MD5)

SHA-256

Yes

SHA-512

Yes

True Random Number Generator (TRNG)

Yes

ISP (Image SigNAl Processing)

Hardware accelerated ISP for RGB and IR

Yes

Deep Learning

Hardware accelerated deep learning

Yes