2.3. Yocto Layer ConfigurationΒΆ

Processor SDK uses the following oe-layersetup configs to configure the meta layers. These are the <config> used in the command:

$ ./oe-layertool-setup.sh -f <config>

The following config files are located in the configs/processor-sdk directory of the oe-layersetup git repo.

Config File

Description

Supported machines/platforms

processor-sdk-09.01.00-legacy-config.txt

Processor SDK 09.01.00.01 Release

am335x-evm, am437x-evm