3.6. Android Low Power Support¶
This application note contains steps to enable low power support in BSP.
Supported low power mode:
- Suspend to RAM (S2R): All power domains are off except for wake-up domain that has wake-up co-processor (DM R5) running. DDR is in self refresh.
3.6.1. Enable Suspend/Resume support¶
Edit android build system
- Update
device/ti/am62xand apply this change:
diff --git a/device-common.mk b/device-common.mk index b111bbc332e5..22c75bfadf31 100644 --- a/device-common.mk +++ b/device-common.mk @@ -238,7 +238,6 @@ PRODUCT_COPY_FILES += \ PRODUCT_COPY_FILES += \ device/ti/am62x/init.am62x.rc:$(TARGET_COPY_OUT_VENDOR)/etc/init/hw/init.$(PRODUCT_PLATFORM).rc \ - device/ti/am62x/init.am62x.zygote_wakelock.rc:$(TARGET_COPY_OUT_VENDOR)/etc/init/init.$(PRODUCT_PLATFORM).zygote_wakelock.rc \ device/ti/am62x/init.am62x.usb.rc:$(TARGET_COPY_OUT_VENDOR)/etc/init/init.$(PRODUCT_PLATFORM).usb.rc \ device/ti/am62x/ueventd.am62x.rc:$(TARGET_COPY_OUT_VENDOR)/etc/ueventd.rc
- Update
At Android prompt, using RTC as wake-up source, test S2R using following command:
console:/ # rtcwake -s 10 -m mem wakeup using "mem" from /dev/rtc0 at Tue Dec 5 18:33:50 2023 [ 95.695175][ T1849] PM: suspend entry (deep) [ 95.703599][ T1849] Filesystems sync: 0.004 seconds [ 95.717906][ T130] ueventd: LoadWithAliases was unable to load rpmsg:rpmsg_ctrl [ 95.726350][ T130] ueventd: LoadWithAliases was unable to load rpmsg:rpmsg_ns [ 95.732045][ T1849] remoteproc remoteproc2: stopped remote processor 5000000.m4fss [ 95.734338][ T130] ueventd: LoadWithAliases was unable to load rpmsg:ti.ipc4.ping-pong [ 95.742092][ T1849] Freezing user space processes [ 95.751455][ T130] ueventd: LoadWithAliases was unable to load rpmsg:rpmsg_chrdev [ 95.765034][ T1849] Freezing user space processes completed (elapsed 0.011 seconds) [ 95.772742][ T1849] OOM killer disabled. [ 95.776670][ T1849] Freezing remaining freezable tasks [ 95.785716][ T1849] Freezing remaining freezable tasks completed (elapsed 0.003 seconds) [ 95.793846][ T1849] printk: Suspending console(s) (use no_console_suspend to debug) [ 95.821084][ T1849] omap8250 2800000.serial: PM domain pd:146 will not be powered off [ 95.830378][ T74] android_work: sent uevent USB_STATE=DISCONNECTED [ 95.849319][ T1849] Disabling non-boot CPUs ... [ 95.851966][ T1849] psci: CPU1 killed (polled 4 ms) [ 95.859202][ T1849] psci: CPU2 killed (polled 0 ms) [ 95.863988][ T1849] psci: CPU3 killed (polled 4 ms) [ 95.866492][ C0] PM: pm_system_irq_wakeup: 240 triggered 2b1f0000.rtc [ 95.866603][ T1849] Enabling non-boot CPUs ... [ 95.867110][ T0] Detected VIPT I-cache on CPU1 [ 95.867180][ T0] GICv3: CPU1: found redistributor 1 region 0:0x00000000018a0000 [ 95.867254][ T0] CPU1: Booted secondary processor 0x0000000001 [0x410fd034] [ 95.869278][ T1849] CPU1 is up [ 95.869698][ T0] Detected VIPT I-cache on CPU2 [ 95.869762][ T0] GICv3: CPU2: found redistributor 2 region 0:0x00000000018c0000 [ 95.869840][ T0] CPU2: Booted secondary processor 0x0000000002 [0x410fd034] [ 95.871633][ T1849] CPU2 is up [ 95.872166][ T0] Detected VIPT I-cache on CPU3 [ 95.872235][ T0] GICv3: CPU3: found redistributor 3 region 0:0x00000000018e0000 [ 95.872312][ T0] CPU3: Booted secondary processor 0x0000000003 [0x410fd034] [ 95.874544][ T1849] CPU3 is up [ 95.875533][ T1849] ti-sci 44043000.system-controller: ti_sci_resume: wakeup source: 0x50 [ 96.112364][ T1849] am65-cpsw-nuss 8000000.ethernet: set new flow-id-base 19 [ 96.118882][ T1849] am65-cpsw-nuss 8000000.ethernet eth0: PHY [8000f00.mdio:00] driver [Generic PHY] (irq=POLL) [ 96.118920][ T1849] am65-cpsw-nuss 8000000.ethernet eth0: configuring for phy/rgmii-rxid link mode [ 96.122398][ T1849] am65-cpsw-nuss 8000000.ethernet eth1: PHY [8000f00.mdio:01] driver [Generic PHY] (irq=POLL) [ 96.122442][ T1849] am65-cpsw-nuss 8000000.ethernet eth1: configuring for phy/rgmii-rxid link mode [ 96.291499][ T1849] OOM killer enabled. [ 96.295346][ T1849] Restarting tasks ... [ 96.298020][ T130] ueventd: LoadWithAliases was unable to load virtio:d00000007v00000000 [ 96.303187][ T1849] done. [ 96.311720][ T130] ueventd: LoadWithAliases was unable to load platform:rproc-virtio [ 96.315356][ T114] android_work: sent uevent USB_STATE=CONNECTED [ 96.329971][ T1849] random: crng reseeded on system resumption [ 96.336133][ T1849] Resume caused by IRQ 240, 2b1f0000.rtc [ 96.340093][ T130] ueventd: LoadWithAliases was unable to load of:Nethernet-phyT(null) [ 96.343128][ T1849] remoteproc remoteproc2: powering up 5000000.m4fss [ 96.355258][ T130] ueventd: LoadWithAliases was unable to load of:Nethernet-phyT(null) [ 96.390489][ T542] dwc3 31000000.usb: request 0000000000000000 was not queued to ep0out [ 96.399033][ T1879] android_work: sent uevent USB_STATE=DISCONNECTED [ 96.400681][ T557] read descriptors [ 96.409119][ T557] read strings [ 96.505086][ T1849] remoteproc remoteproc2: Booting fw image am62-mcu-m4f0_0-fw, size 55016 [ 96.515404][ T1849] rproc-virtio rproc-virtio.4.auto: assigned reserved memory node m4f-dma-memory@9cb00000 [ 96.518238][ T130] ueventd: LoadWithAliases was unable to load platform:rproc-virtio [ 96.526698][ T1849] virtio_rpmsg_bus virtio0: rpmsg host is online [ 96.537008][ T130] ueventd: LoadWithAliases was unable to load platform:rproc-virtio [ 96.539484][ T96] virtio_rpmsg_bus virtio0: creating channel ti.ipc4.ping-pong addr 0xd console:/ # [ 96.543700][ T1849] rproc-virtio rproc-virtio.4.auto: registered virtio0 (type 7) [ 96.543731][ T1849] remoteproc remoteproc2: remote processor 5000000.m4fss is now up [ 96.543796][ T1849] PM: suspend exit [ 96.551052][ T130] ueventd: LoadWithAliases was unable to load virtio:d00000007v00000000 [ 96.556102][ T96] virtio_rpmsg_bus virtio0: creating channel rpmsg_chrdev addr 0xe [ 96.567673][ T130] ueventd: LoadWithAliases was unable to load rpmsg:rpmsg_ctrl [ 96.602513][ T130] ueventd: LoadWithAliases was unable to load rpmsg:rpmsg_ns [ 96.613150][ T130] ueventd: LoadWithAliases was unable to load rpmsg:rpmsg_ns [ 96.623603][ T130] ueventd: LoadWithAliases was unable to load virtio:d00000007v00000000 [ 96.635333][ T130] ueventd: LoadWithAliases was unable to load rpmsg:ti.ipc4.ping-pong [ 96.646928][ T130] ueventd: LoadWithAliases was unable to load rpmsg:rpmsg_chrdev [ 96.661957][ T130] ueventd: LoadWithAliases was unable to load rpmsg:rpmsg_chrdev [ 97.260423][ T96] android_work: sent uevent USB_STATE=CONNECTED [ 97.415786][ T96] android_work: sent uevent USB_STATE=CONFIGURED
This puts system to sleep for 10s and then wakes it up via RTC interrupt.