1.3. Flashing Instruction
1.3.1. DFU Recovery
It’s possible to put the AM62Px SK EVM in USB DFU mode, which allows
loading bootloaders over DFU. This is done via the snagboot tool.
This is useful for initial flashing or recovering boards which have broken bootloaders.
1.3.1.1. Installation and setup
Install snagboot following the official instructions
Note
If Snagboot cannot be installed, it’s possible boot the initial bootloaders from an SD card.
Follow Android Bootloader on SD Card if you encounter issues with Snagboot.
1.3.2. eMMC flashing
1.3.2.1. Flashing instructions
Once the build is complete, follow the steps below to flash the images to eMMC.
Change the boot mode DIP switches to DFU mode:
Switch Label
SW2: 12345678
SW3: 12345678
USB DFU
00000000
11001010
Ensure the device is plugged in with USB host and debug UART/serial debug
Open a terminal debugger to view console output from the device:
$ sudo picocom -b 115200 -r -l /dev/ttyUSB0
run
snagrecoverfor host
# If you are using binaries built locally $ cd out/target/product/am62p (OR) # If you are using pre-built binaries from SDK download page $ cd AM62Px_09.02.00_emmc $ snagrecover -s am625 -f ./am62px-sk-evm-hsfs.yamlIn the serial console, you will see:
SYSFW ABI: 3.1 (firmware rev 0x0009 '9.0.5--v09.00.05 (Kool Koala)') SPL initial stack usage: 1856 bytes Trying to boot from DFU
Setup default U-Boot environment
Type
Ctrl-Cin the serial console to continue to U-Boot. From there, we should ensure the default U-Boot environment is configured with:=> env default -f -a; saveenv;Note
If you build with TARGET_AVB_ENABLE=true or flash user images you need to do this command in U-Boot console:
=> setenv force_avb "1"; saveenv;Note
By default, no Device-Tree Overlays are selected. Follow this link to configure Device Tree Overlay Support
Enable fastboot mode on the device through the terminal debugger by executing below command. Before running this command make sure USB-C cable is connected from the host PC to the EVM:
=> fastboot 0From the host PC run the
flashall.shscript to start flashing the binaries to eMMC:
# If you are using binaries built locally $ cd out/target/product/am62p (OR) # If you are using pre-built binaries from SDK download page $ cd AM62Px_09.02.00_emmc $ sudo ./flashall.sh --board am62px-skNote
If you get
mcopycommand not found error on Linux PC, install themtoolspackage:$ apt-get install mtoolsWarning
It’s possible that the in-memory partition layout is still from an older system. In that case, we can observe flashing errors similar to:
writing 'tiboot3'... FAILED (remote: invalid partition or device)When that happens:
Reboot into the newfly flashed bootloader with
$ fastboot reboot bootloaderRestart the flashing from step 5.
Once the flashing is complete, power off the board
Change boot mode DIP switches to boot from eMMC user partitions and power cycle the board:
Switch Label
SW2: 12345678
SW3: 12345678
EMMC (with UDA)
00000000
11000010
Board should boot the Android images now.
1.3.3. Flashing the kernel
In order to flash a new kernel, the new boot image should be flashed:
$ adb reboot bootloader
< Wait for bootloader reboot >
$ cd <PATH/TO/BOOT/IMAGE>
$ fastboot flash boot boot.img
$ fastboot reboot
The board should boot with the new kernel build.