Contains the public interface to the stator voltage frequency generator (VS_FREQ)
Go to the source code of this file.
Data Structures | |
struct | VS_FREQ_Handle |
Defines the angle generator (ANGLE_COMP) object. More... | |
Functions | |
static float32_t | VS_FREQ_getVd_out (VS_FREQ_Handle handle) |
Gets the Vd output value in VS_FREQ. More... | |
static float32_t | VS_FREQ_getVq_out (VS_FREQ_Handle handle) |
static void | VS_FREQ_setMaxFreq (VS_FREQ_Handle handle, float32_t maxFreq) |
Sets the parameters maximum frequency. More... | |
static void | VS_FREQ_setVsMagPu (VS_FREQ_Handle handle, float32_t maxVsMag_pu) |
Sets the parameters VsMag_pu. More... | |
void | VS_FREQ_setProfile (VS_FREQ_Handle handle, float32_t LowFreq, float32_t HighFreq, float32_t VoltMin, float32_t VoltMax) |
Sets the parameters. More... | |
VS_FREQ_Handle | VS_FREQ_init (void *pMemory, const size_t numBytes) |
Initializes the angle generator (VS_FREQ) module. More... | |
static void | VS_FREQ_run (VS_FREQ_Handle handle, const float32_t Freq_pu) |
Generates an output command voltage for a specific input command frequency according to the specified volts/hertz profile. More... | |