AM263x Motor Control SDK  09.02.00

Introduction

Contains phase voltage calculation (VOLREC) functions implementation.

Go to the source code of this file.

Data Structures

struct  VOLREC_Obj
 Defines the VOLREC controller object. More...
 

Typedefs

typedef struct _VOLREC_Obj_ * VOLREC_Handle
 Defines the VOLREC_Handle. More...
 

Functions

VOLREC_Handle VOLREC_init (void *pMemory, const size_t numBytes)
 Initializes the Voltage reconstruct module. More...
 
void VOLREC_reset (VOLREC_Handle handle)
 reset the Phase Voltage reconstruction variables More...
 
void VOLREC_setParams (VOLREC_Handle handle, const float32_t filterPole_rps, const float32_t ctrlFreq_Hz)
 set the Phase Voltage reconstruction parameters More...
 
static void VOLREC_calcVolSF (VOLREC_Handle handle, float32_t VaSen)
 Runs the Phase Voltage reconstruction. More...
 
static void VOLREC_run (VOLREC_Handle handle, float32_t Vdcbus, MATH_Vec3 *pVin, MATH_Vec2 *pVab)
 Runs the Phase Voltage reconstruction. More...
 
static bool VOLREC_getFlagCalSf (VOLREC_Handle handle)
 Gets the SF enable flag. More...
 
static void VOLREC_setFlagCalSf (VOLREC_Handle handle, const bool flagCalSf)
 Sets up the SF enable flag. More...
 
static void VOLREC_enableFlagCalSf (VOLREC_Handle handle)
 Enables the SF enable flag. More...
 
static void VOLREC_disableFlagEnableSf (VOLREC_Handle handle)
 Disables the SF enable flag. More...