Defines the VOLREC controller object.
Data Fields | |
float32_t | a1 |
the denominator filter coefficient value for z^(-1) More... | |
float32_t | b0 |
the numerator filter coefficient value for z^0 More... | |
float32_t | b1 |
the numerator filter coefficient value for z^(-1) More... | |
MATH_Vec3 | x1 |
the input value at time sample n=-1 More... | |
MATH_Vec3 | y1 |
the output value at time sample n=-1 More... | |
MATH_Vec3 | Vin_V |
the input Phase voltage phase (V) More... | |
MATH_Vec3 | Vs_V |
the input Phase voltage phase (V) More... | |
float32_t | sf |
the scale factor of phase voltage More... | |
float32_t | sfCalc |
the scale factor of phase voltage More... | |
float32_t | threshold |
the voltage level corresponding to zero i/p More... | |
float32_t | VaSen |
the input Phase voltage phase (V) More... | |
float32_t | VaSenSum |
the square calculation over one sine cycle More... | |
float32_t | VaSum |
the square calculation over one sine cycle More... | |
float32_t | VaSenRms |
the RMS Value More... | |
float32_t | VaRms |
the RMS Value More... | |
int32_t | numSamples |
the sampling points More... | |
int32_t | minSamples |
the sampling points More... | |
int32_t | maxSamples |
the sampling points More... | |
int32_t | signPrev |
the flag to detect ZCD More... | |
int32_t | signCurr |
the flag to detect ZCD More... | |
int32_t | jitterCount |
the jitter count due to noise on input More... | |
bool | flagCalSf |
float32_t VOLREC_Obj::a1 |
the denominator filter coefficient value for z^(-1)
float32_t VOLREC_Obj::b0 |
the numerator filter coefficient value for z^0
float32_t VOLREC_Obj::b1 |
the numerator filter coefficient value for z^(-1)
MATH_Vec3 VOLREC_Obj::x1 |
the input value at time sample n=-1
MATH_Vec3 VOLREC_Obj::y1 |
the output value at time sample n=-1
MATH_Vec3 VOLREC_Obj::Vin_V |
the input Phase voltage phase (V)
MATH_Vec3 VOLREC_Obj::Vs_V |
the input Phase voltage phase (V)
float32_t VOLREC_Obj::sf |
the scale factor of phase voltage
float32_t VOLREC_Obj::sfCalc |
the scale factor of phase voltage
float32_t VOLREC_Obj::threshold |
the voltage level corresponding to zero i/p
float32_t VOLREC_Obj::VaSen |
the input Phase voltage phase (V)
float32_t VOLREC_Obj::VaSenSum |
the square calculation over one sine cycle
float32_t VOLREC_Obj::VaSum |
the square calculation over one sine cycle
float32_t VOLREC_Obj::VaSenRms |
the RMS Value
float32_t VOLREC_Obj::VaRms |
the RMS Value
int32_t VOLREC_Obj::numSamples |
the sampling points
int32_t VOLREC_Obj::minSamples |
the sampling points
int32_t VOLREC_Obj::maxSamples |
the sampling points
int32_t VOLREC_Obj::signPrev |
the flag to detect ZCD
int32_t VOLREC_Obj::signCurr |
the flag to detect ZCD
int32_t VOLREC_Obj::jitterCount |
the jitter count due to noise on input
bool VOLREC_Obj::flagCalSf |