Contains speed calculation functions.
Go to the source code of this file.
Data Structures | |
struct | SPDCALC_Obj |
Typedefs | |
typedef struct _SPDCALC_obj_ * | SPDCALC_Handle |
Defines the ESMO handle. More... | |
Functions | |
SPDCALC_Handle | SPDCALC_init (void *pMemory, const size_t numBytes) |
Set the SPDCALC controller. More... | |
void | SPDCALC_reset (SPDCALC_Handle handle) |
Set the SPDCALC controller. More... | |
void | SPDCALC_setParams (SPDCALC_Handle handle, const USER_Params *pUserParams) |
Set the SPDCALC controller. More... | |
static float32_t | SPDCALC_getSpeedHz (SPDCALC_Handle handle) |
Set the SPDCALC controller. More... | |
static void | SPDCALC_run (SPDCALC_Handle handle, float32_t theta) |
Set the SPDCALC controller. More... | |