AM263x Motor Control SDK  09.02.00

Introduction

PI (Proportional and Integral) controller library.

Note
This library is meant to be API backwards-compatible with existing software. It uses DCL (digital control library)'s PI controller located in SDK's source/dcl folder.

Go to the source code of this file.

Data Structures

struct  PI_Obj
 Defines the PI controller object. More...
 

Typedefs

typedef struct _PI_Obj_ * PI_Handle
 Defines the PI handle. More...
 

Functions

static float32_t PI_getFbackValue (PI_Handle handle)
 Gets the feedback value in the PI controller. More...
 
static float32_t PI_getFfwdValue (PI_Handle handle)
 Gets the feedforward value in the PI controller. More...
 
static void PI_getGains (PI_Handle handle, float32_t *pKp, float32_t *pKi)
 Gets the gains in the PI controller. More...
 
static float32_t PI_getKi (PI_Handle handle)
 Gets the integral gain in the PI controller. More...
 
static float32_t PI_getKp (PI_Handle handle)
 Gets the proportional gain in the PI controller. More...
 
static void PI_getMinMax (PI_Handle handle, float32_t *pOutMin, float32_t *pOutMax)
 Gets the minimum and maximum output value allowed in the PI controller. More...
 
static float32_t PI_getOutMax (PI_Handle handle)
 Gets the maximum output value allowed in the PI controller. More...
 
static float32_t PI_getOutMin (PI_Handle handle)
 Gets the minimum output value allowed in the PI controller. More...
 
static float32_t PI_getRefValue (PI_Handle handle)
 Gets the reference value in the PI controller. More...
 
static float32_t PI_getUi (PI_Handle handle)
 Gets the integrator start value in the PI controller. More...
 
PI_ObjPI_init (void *pMemory, const size_t numBytes)
 Initializes the PI controller. More...
 
static void PI_setFbackValue (PI_Handle handle, const float32_t fbackValue)
 Sets the feedback value in the PI controller. More...
 
static void PI_setFfwdValue (PI_Handle handle, const float32_t ffwdValue)
 Sets the feedforward value in the PI controller. More...
 
static void PI_setGains (PI_Handle handle, const float32_t Kp, const float32_t Ki)
 Sets the gains in the PI controller. More...
 
static void PI_setKi (PI_Handle handle, const float32_t Ki)
 Sets the integral gain in the PI controller. More...
 
static void PI_setKp (PI_Handle handle, const float32_t Kp)
 Sets the proportional gain in the PI controller. More...
 
static void PI_setMinMax (PI_Handle handle, const float32_t outMin, const float32_t outMax)
 Sets the minimum and maximum output value allowed in the PI controller. More...
 
static void PI_setOutMax (PI_Handle handle, const float32_t outMax)
 Sets the maximum output value allowed in the PI controller. More...
 
static void PI_setOutMin (PI_Handle handle, const float32_t outMin)
 Sets the minimum output value allowed in the PI controller. More...
 
static void PI_setRefValue (PI_Handle handle, const float32_t refValue)
 Sets the reference value in the PI controller. More...
 
static void PI_setUi (PI_Handle handle, const float32_t Ui)
 Sets the integrator start value in the PI controller. More...
 
static void PI_run_parallel (PI_Handle handle, const float32_t refValue, const float32_t fbackValue, const float32_t ffwdValue, float32_t *pOutValue)
 Runs the parallel form of the PI controller. More...
 
static void PI_run_series (PI_Handle handle, const float32_t refValue, const float32_t fbackValue, const float32_t ffwdValue, float32_t *pOutValue)
 Runs the series form of the PI controller. More...
 
static void PI_run (PI_Handle handle, const float32_t refValue, const float32_t fbackValue, float32_t *pOutValue)
 Runs the series form of the PI controller without updating the data strcture. More...