AM243x Motor Control SDK  11.00.00
APIs for Maximum Torque Per Ampere (MTPA)

Introduction

Here is the list of FWC function APIs

Files

file  mtpa.h
 Contains Maximum torque per ampere (MTPA) functions implementation.
 

Data Structures

struct  MTPA_Handle
 Defines the MTPA object. More...
 

Functions

void MTPA_computeParameters (MTPA_Handle handle, const float32_t Ls_d_H, const float32_t Ls_q_H, const float32_t flux_Wb)
 Computes the motor constant for MTPA module. More...
 
MTPA_Handle MTPA_init (void *pMemory, const size_t numBytes)
 Initializes the maximum torque per ampere (MTPA) module. More...
 
static void MTPA_disable (MTPA_Handle handle)
 Disables the MTPA. More...
 
static void MTPA_enable (MTPA_Handle handle)
 Enables the MTPA. More...
 
static float32_tMTPA_getCurrentAnglePhase_rad_addr (MTPA_Handle handle)
 Gets the stator current phase angle memory address. More...
 
static float32_t MTPA_getCurrentAngle_rad (MTPA_Handle handle)
 Gets the stator current phase angle value (angleCurrent_rad) More...
 
static float32_t MTPA_getKconst (MTPA_Handle handle)
 Gets the motor constant of MTPA. More...
 
static float32_tMTPA_getIs_ref_A_addr (MTPA_Handle handle)
 Gets the stator current reference memory address. More...
 
static bool MTPA_getFlagEnable (MTPA_Handle handle)
 Gets the enable controller flag value from the controller. More...
 
static float32_t MTPA_getId_ref_A (MTPA_Handle handle)
 Gets the direct current reference value (Id_ref_A) More...
 
static float32_t MTPA_getIq_ref_A (MTPA_Handle handle)
 Gets the quadrature current reference value (Iq_ref_A) More...
 
static float32_t MTPA_getIs_ref_A (MTPA_Handle handle)
 Gets the stator current reference value (Is_ref_A) More...
 
static void MTPA_setFlagEnable (MTPA_Handle handle, const bool flagEnable)
 Sets the enable flag. More...
 
static void MTPA_setCurrentAngle_rad (MTPA_Handle handle, const float32_t angleCurrent_rad)
 Sets the stator current phase angle value. More...
 
static void MTPA_setId_ref_A (MTPA_Handle handle, const float32_t Id_ref_A)
 Sets the direct current (Id_ref) reference vector value. More...
 
static void MTPA_setIq_ref_A (MTPA_Handle handle, const float32_t Iq_ref_A)
 Sets the quadrature current (Iq_ref) reference value. More...
 
static void MTPA_setIs_ref_A (MTPA_Handle handle, const float32_t Is_ref_A)
 Sets the stator current reference value (Is_ref) More...
 
static float32_t MTPA_updateLs_d_withLUT (MTPA_Handle handle, const float32_t Is_A)
 Update the motor inductances. More...
 
static float32_t MTPA_updateLs_q_withLUT (MTPA_Handle handle, const float32_t Is_A)
 Update the motor inductances. More...
 
static void MTPA_computeCurrentReference (MTPA_Handle handle, const float32_t Is_ref_A)
 Compute the current reference of MTPA. More...
 
static float32_t MTPA_computeCurrentAngle (MTPA_Handle handle, const float32_t Is_ref_A)
 Compute the current angle of MTPA. More...
 

Macros

#define MTPA_LUT_INDEX_LD_MAX   20
 Defines the maximum length of LUT for Ld. More...
 
#define MTPA_LUT_INDEX_LQ_MAX   20
 Defines the maximum length of LUT for Lq. More...
 
#define MTPA_LUT_DELTA_CURRENT_LD_A   0.5
 Defines the current delta of LUT for Ld, A. More...
 
#define MTPA_LUT_DELTA_CURRENT_LD_A   0.5
 Defines the current delta of LUT for Ld, A. More...
 

Macro Definition Documentation

◆ MTPA_LUT_INDEX_LD_MAX

#define MTPA_LUT_INDEX_LD_MAX   20

Defines the maximum length of LUT for Ld.

◆ MTPA_LUT_INDEX_LQ_MAX

#define MTPA_LUT_INDEX_LQ_MAX   20

Defines the maximum length of LUT for Lq.

◆ MTPA_LUT_DELTA_CURRENT_LD_A [1/2]

#define MTPA_LUT_DELTA_CURRENT_LD_A   0.5

Defines the current delta of LUT for Ld, A.

Defines the current delta of LUT for Lq, A.

◆ MTPA_LUT_DELTA_CURRENT_LD_A [2/2]

#define MTPA_LUT_DELTA_CURRENT_LD_A   0.5

Defines the current delta of LUT for Ld, A.

Defines the current delta of LUT for Lq, A.

Function Documentation

◆ MTPA_computeParameters()

void MTPA_computeParameters ( MTPA_Handle  handle,
const float32_t  Ls_d_H,
const float32_t  Ls_q_H,
const float32_t  flux_Wb 
)

Computes the motor constant for MTPA module.

Parameters
[in]handleThe maximum torque per ampere (MTPA) handle
[in]Ls_d_HThe direct stator inductance, Henry
[in]Ls_q_HThe quadrature stator inductance, Henry
[in]flux_WbThe rated flux value, Wb

◆ MTPA_init()

MTPA_Handle MTPA_init ( void *  pMemory,
const size_t  numBytes 
)

Initializes the maximum torque per ampere (MTPA) module.

Parameters
[in]pMemoryA pointer to the memory for the MTPA object
[in]numBytesThe number of bytes allocated for the MTPA object
Returns
The Maximum torque per ampere (MTPA) object handle

◆ MTPA_disable()

static void MTPA_disable ( MTPA_Handle  handle)
inlinestatic

Disables the MTPA.

Parameters
[in]handleThe maximum torque per ampere (MTPA) handle

◆ MTPA_enable()

static void MTPA_enable ( MTPA_Handle  handle)
inlinestatic

Enables the MTPA.

Parameters
[in]handleThe maximum torque per ampere (MTPA) handle

◆ MTPA_getCurrentAnglePhase_rad_addr()

static float32_t* MTPA_getCurrentAnglePhase_rad_addr ( MTPA_Handle  handle)
inlinestatic

Gets the stator current phase angle memory address.

Parameters
[in]handleThe maximum torque per ampere (MTPA) handle
Returns
The stator current phase angle memory address

◆ MTPA_getCurrentAngle_rad()

static float32_t MTPA_getCurrentAngle_rad ( MTPA_Handle  handle)
inlinestatic

Gets the stator current phase angle value (angleCurrent_rad)

Parameters
[in]handleThe maximum torque per ampere (MTPA) handle
Returns
The stator current phase angle value, rad

◆ MTPA_getKconst()

static float32_t MTPA_getKconst ( MTPA_Handle  handle)
inlinestatic

Gets the motor constant of MTPA.

Parameters
[in]handleThe maximum torque per ampere (MTPA) handle
Returns
The motor constant of MTPA

◆ MTPA_getIs_ref_A_addr()

static float32_t* MTPA_getIs_ref_A_addr ( MTPA_Handle  handle)
inlinestatic

Gets the stator current reference memory address.

Parameters
[in]handleThe maximum torque per ampere (MTPA) handle
Returns
The stator current reference memory address

◆ MTPA_getFlagEnable()

static bool MTPA_getFlagEnable ( MTPA_Handle  handle)
inlinestatic

Gets the enable controller flag value from the controller.

Parameters
[in]handleThe maximum torque per ampere (MTPA) handle
Returns
The enable MTPA flag value

◆ MTPA_getId_ref_A()

static float32_t MTPA_getId_ref_A ( MTPA_Handle  handle)
inlinestatic

Gets the direct current reference value (Id_ref_A)

Parameters
[in]handleThe maximum torque per ampere (MTPA) handle
Returns
The direct reference reference current, A

◆ MTPA_getIq_ref_A()

static float32_t MTPA_getIq_ref_A ( MTPA_Handle  handle)
inlinestatic

Gets the quadrature current reference value (Iq_ref_A)

Parameters
[in]handleThe maximum torque per ampere (MTPA) handle
Returns
The quadrature current reference value, A

◆ MTPA_getIs_ref_A()

static float32_t MTPA_getIs_ref_A ( MTPA_Handle  handle)
inlinestatic

Gets the stator current reference value (Is_ref_A)

Parameters
[in]handleThe maximum torque per ampere (MTPA) handle
Returns
The stator current reference value, A

◆ MTPA_setFlagEnable()

static void MTPA_setFlagEnable ( MTPA_Handle  handle,
const bool  flagEnable 
)
inlinestatic

Sets the enable flag.

Parameters
[in]handleThe maximum torque per ampere (MTPA) handle
[in]flagEnableThe enable flag

◆ MTPA_setCurrentAngle_rad()

static void MTPA_setCurrentAngle_rad ( MTPA_Handle  handle,
const float32_t  angleCurrent_rad 
)
inlinestatic

Sets the stator current phase angle value.

Parameters
[in]handleThe maximum torque per ampere (MTPA) handle
[in]angleCurrent_radThe stator current phase angle value, rad

◆ MTPA_setId_ref_A()

static void MTPA_setId_ref_A ( MTPA_Handle  handle,
const float32_t  Id_ref_A 
)
inlinestatic

Sets the direct current (Id_ref) reference vector value.

Parameters
[in]handleThe maximum torque per ampere (MTPA) handle
[in]Id_ref_AThe direct current reference value, A

◆ MTPA_setIq_ref_A()

static void MTPA_setIq_ref_A ( MTPA_Handle  handle,
const float32_t  Iq_ref_A 
)
inlinestatic

Sets the quadrature current (Iq_ref) reference value.

Parameters
[in]handleThe maximum torque per ampere (MTPA) handle
[in]Iq_ref_AThe quadrature current reference value, A

◆ MTPA_setIs_ref_A()

static void MTPA_setIs_ref_A ( MTPA_Handle  handle,
const float32_t  Is_ref_A 
)
inlinestatic

Sets the stator current reference value (Is_ref)

Parameters
[in]handleThe maximum torque per ampere (MTPA) handle
[in]Is_ref_AThe stator current reference value, A

◆ MTPA_updateLs_d_withLUT()

static float32_t MTPA_updateLs_d_withLUT ( MTPA_Handle  handle,
const float32_t  Is_A 
)
inlinestatic

Update the motor inductances.

Parameters
[in]handleThe maximum torque per ampere (MTPA) handle
[in]Is_AThe stator current value, A
Returns
The d-axis inductance

◆ MTPA_updateLs_q_withLUT()

static float32_t MTPA_updateLs_q_withLUT ( MTPA_Handle  handle,
const float32_t  Is_A 
)
inlinestatic

Update the motor inductances.

Parameters
[in]handleThe maximum torque per ampere (MTPA) handle
[in]Is_AThe stator current value, A
Returns
The q-axis inductance

◆ MTPA_computeCurrentReference()

static void MTPA_computeCurrentReference ( MTPA_Handle  handle,
const float32_t  Is_ref_A 
)
static

Compute the current reference of MTPA.

Parameters
[in]handleThe maximum torque per ampere (MTPA) handle
[in]Is_ref_AThe stator current reference value, A

◆ MTPA_computeCurrentAngle()

static float32_t MTPA_computeCurrentAngle ( MTPA_Handle  handle,
const float32_t  Is_ref_A 
)
static

Compute the current angle of MTPA.

Parameters
[in]handleThe maximum torque per ampere (MTPA) handle
[in]Is_ref_AThe stator current reference value, A
Returns
The vector stator current reference

Variable Documentation

◆ MTPA_Ld_tableData_H

const float32_t MTPA_Ld_tableData_H[MTPA_LUT_INDEX_LD_MAX+1]
extern

Defines the Ld array.

◆ MTPA_Lq_tableData_H

const float32_t MTPA_Lq_tableData_H[MTPA_LUT_INDEX_LQ_MAX+1]
extern

Defines the Lq array.