Various industries like Robotics, Industrial Automation, Manufacturing processes, CNC Machining, and Medical Devices require accurate and precise position control. Multiple UART-based encoder protocols in the market help to effectively measure position, speed, and direction of motion in various systems. It is a challenge to interface the different UART based encoders with a host processor in a multi-channel fashion due to factors like different data sizes and different baud rates used in various protocols.
The aim of this document is to showcase the capabilities of the Three Channel Peripheral Interface in PRU-ICSS on Sitara™ processors/microcontrollers and to show steps for achieving a solution for interfacing different UART based encoders in the market and also provide flexibility in selection of baud rates for the encoder communication. The same solution can also be used for general purpose UART like debugging, logging, etc. For more details on Three Channel Peripheral Interface of PRU-ICSS, please see section "6.4.5.2.2.3.6 Three Channel Peripheral Interface" of AM243x Technical Reference Manual.
There are three main reasons when it comes to creating a programmable software based solution for a custom multi-channel UART encoder interface:
This SDK contains software (which runs on Arm®-based core) and firmware (which runs on PRU-ICSS) which implement the interface for Tamagawa encoders. More details on Tamagawa implementation can be found in Tamagawa and Tamagawa Protocol Design pages.
There are three aspects of this firmware + software solution :
Firmware sources for Tamagawa are available in "${SDK_INSTALL_PATH}/source/position_sense/tamagawa/firmware" folder.
Following are different aspects of firmware which can be tweaked in firmware based on the need of custom UART implementation.
Firstly, initialization is done as shown in Initialization. Then the configuration for send and receive is done as shown in Transmit and Receive.
PRU-ICSS supports an internal wrapper multiplexing that expands the device top-level multiplexing. This wrapper multiplexing is controlled by the GPCFGx_REG register (where x = 0 or 1) in the PRU-ICSS CFG register space and allows MII_RT, 3 channel Peripheral Interface, and Sigma Delta functionality to be muxed with the PRU GPI/O device signals. For this use-case, 3 channel Peripheral Interface should be configured.
TAMAGAWA_INIT in "${SDK_INSTALL_PATH}/source/position_sense/tamagawa/firmware/tamagawa_main.asm"Communication is needed between Arm-based core and PRUs. For this purpose, data memory of PRU-ICSS is typically used. The memory map of this shared memory region for Tamagawa is defined in one file. Based on the need, this memory map can be updated to add or remove data variables as per the need.
The Peripheral Interface module has two source clock options, ICSSGn_UART_CLK (default) and ICSSGn_ICLK. There are two independent clock dividers (div16) for the 1x and oversampling (OS) clocks, and each clock divider is configurable by two cascading dividers in ICSSG_PRUx_ED_RX_CFG_REG and ICSSG_PRU0_ED_TX_CFG_REG registers.
The 1x clock is output on the clock signal. In TX mode, the output data is read from the TX FIFO at this 1x clock rate. In RX mode, the input data is sampled at the OS clock rate.Multiple options are available for start and stop conditions for the clock.
For more details on clocking capabilities and configuration, please see section "6.4.5.2.2.3.6.3 Clock Generation" of AM243x Technical Reference Manual.
TAMAGAWA_SET_CLOCK, and FN_SET_TX_CLK in "${SDK_INSTALL_PATH}/source/position_sense/tamagawa/firmware/tamagawa_main.asm"For Tamagawa, this configuration is done for 2.5 MHz or 5 MHz based on the encoder being used.
After initialization, the firmware checks whether it is host trigger mode or periodic trigger mode. In host trigger mode, it waits until a command has been triggered through the share memory interface from Arm-based core. In periodic trigger mode, the firmware sets host trigger bit based on PRU-ICSS IEP compare event configured. Upon triggering the transmit data is set up and transmitted.
CHECK_OPERATING_MODE, HANDLE_PERIODIC_TRIGGER_MODE, and HANDLE_HOST_TRIGGER_MODE in "${SDK_INSTALL_PATH}/source/position_sense/tamagawa/firmware/tamagawa_main.asm"Now the configuration for sending and receiving data over the interface needs to be done.
FN_SEND configures the size of TX in ICSS_CFG_PRUx_ED_CHx_CFG0 register. This code can be modified to change the size to any number. The TX FIFO size is 32 bits. If more than 32 bits need to be sent, then continuous FIFO loading mode has to be used. In Tamagawa, for EEPROM Write Command this mode is used. FN_SEND configures the size to 10 bits for normal commands, 30 bits for EEPROM Read command and 0 bit for EEPROM Write command (which means continuous mode). For continuous mode, FIFO level should be polled and data should be continuously pushed based on free space. Data is loaded into FIFO and then TX GO is asserted which starts the TX. The flow for transmit in Tamagawa is explained in Setup Transmit Data.RECEIVE_FRAMES_S and RECEIVE_FRAMES_M contain the code for receive. Start bit polarity of RX can be configured in ICSSG_PRUx_ED_RX_CFG_REG. Once this bit is seen on RX pin, the RX FIFO starts filling up. The size of RX needs to configured based on the protocol requirement. The data needs to be fetched from FIFO to ensure that overflow of RX FIFO does not occur. The clock will be stopped based on the clock mode configured before the start of the RX operation. The flow for receive in Tamagawa is explained in Transmit and Receive.For more details on the programming sequence for TX, RX and clock configuration, please see section "6.4.5.2.2.3.6.4 Three Peripheral Mode Basic Programming Model" of AM243x Technical Reference Manual.
When doing TX or RX, FIFO over-run and under-run should be avoided to ensure correct operation.
EEPROM_WRITE_MACRO in Tamagawa firmware uses continuous mode for TX. It loads 32 bits (4 bytes) initially and enables TX. Then once the FIFO Fill Level is below 3 bytes, it pushes one more byte.The time available can be converted into PRU cycles based on the PRU Core Clock Frequency. If PRU Core Clock Frequency is 200 MHz, then one PRU cycle will be 5 ns. Non read and write instructions take exactly one PRU clock cycle to execute. For read and write instructions, there are specific rules for how long a read or a write instruction will take. This is explained in an FAQ "PRU: How do I calculate read and write latencies? "
RECEIVE_FRAMES_S in Tamagawa firmware performs the RX operation for single channel mode.FN_SEND_RECEIVE_TAMAGAWA and FN_SEND in "${SDK_INSTALL_PATH}/source/position_sense/tamagawa/firmware/tamagawa_main.asm"TAMAGAWA_SEND_MACRO in "${SDK_INSTALL_PATH}/source/position_sense/tamagawa/firmware/tamagawa_send.h"RECEIVE_FRAMES_S in "${SDK_INSTALL_PATH}/source/position_sense/tamagawa/firmware/single_ch_receive_frames.h" for single channel receiveRECEIVE_FRAMES_M in "${SDK_INSTALL_PATH}/source/position_sense/tamagawa/firmware/multi_ch_receive_frames.h" for multi channel receiveOn the data received, CRC needs to be computed. The RX code does on-the-fly CRC computation as it is receiving data bits continuously. The computed CRC can then be compared with the CRC from the received data.
For Tamagawa, the CRC polynomial is (x8 + 1).
This code for on-the-fly CRC computation can be modified for any other polynomial as well. The PRU instruction cycle budget requirement will vary based on the polynomial. RX Loop timing should not be broken, else it will lead to RX FIFO overflow (if data is not read fast enough). If on-the-fly CRC computation is not viable, then there are two options. One option is to do CRC computation as a part of post-processing after RX is complete. Second is to check if HW CRC16/32 Module from PRU-ICSS can be used. The CRC16/32 module directly connects with the PRU internal registers R25-R29 through use of the PRU broadside interface and XFR instructions. It supports three different polynomials. For more details, see section "6.4.6.2.2 PRU CRC16/32 Module" of AM243x Technical Reference Manual.
RECEIVE_FRAMES_S in "${SDK_INSTALL_PATH}/source/position_sense/tamagawa/firmware/single_ch_receive_frames.h" for single channel receiveRECEIVE_FRAMES_M in "${SDK_INSTALL_PATH}/source/position_sense/tamagawa/firmware/multi_ch_receive_frames.h" for multi channel receiveDriver layer does communication with PRU core(s) via shared memory. New driver APIs can be added or existing APIs can be updated based on the changes need in this communication.
The APIs for Tamagawa are described in APIs for Tamagawa Encoder.
Tamagawa application does below configures pinmux, UART, PRU-ICSS clock, and loads the the PRU firmware. This application is controlled with a terminal interface using a serial over USB connection between the PC host and the EVM, using which the data transfer can be triggered. The application collects the data entered by the user, configures the relevant interface and sends the command. Once the command completion is indicated by the interface, the status of the transaction is checked. If the Status indicates success, the result is presented to the user.
For a new custom UART application, Tamagawa application is a good starting point as most of the configuration like pinmux, PRU-ICSS initialization, etc. will be same as in Tamagawa. Based on the changes in driver APIs and features implemented in firmware, the API calls can be updated in the application.
Please refer to following documents to understand more about certain topics discussed in this document.
| Document | Description |
|---|---|
| Tamagawa Tamagawa Protocol Design | SDK Documentation for Tamagawa features and design |
| AM243x Technical Reference Manual | Section "6.4.5.2.2.3.6 Three Channel Peripheral Interface" |
| Section "6.4.5.2.2.3.6.3 Clock Generation" | |
| Section 6.4.5.2.2.3.6.4 Three Peripheral Mode Basic Programming Model | |
| Section "6.4.6.2.2 PRU CRC16/32 Module" | |
| PRU: How do I calculate read and write latencies? | FAQ on read and write latencies for PRU Instructions |
| APIs for Tamagawa Encoder | SDK Documentation for Tamagawa Driver APIs |