AM243x Motor Control SDK  09.02.00

Introduction

Contains speed calculation functions.

Go to the source code of this file.

Data Structures

struct  SPDCALC_Obj
 

Typedefs

typedef struct _SPDCALC_obj_ * SPDCALC_Handle
 Defines the ESMO handle. More...
 

Functions

SPDCALC_Handle SPDCALC_init (void *pMemory, const size_t numBytes)
 Set the SPDCALC controller. More...
 
void SPDCALC_reset (SPDCALC_Handle handle)
 Set the SPDCALC controller. More...
 
void SPDCALC_setParams (SPDCALC_Handle handle, const USER_Params *pUserParams)
 Set the SPDCALC controller. More...
 
static float32_t SPDCALC_getSpeedHz (SPDCALC_Handle handle)
 Set the SPDCALC controller. More...
 
static void SPDCALC_run (SPDCALC_Handle handle, float32_t theta)
 Set the SPDCALC controller. More...