![Logo](ti_logo.svg) |
AM243x Motor Control SDK
09.02.00
|
|
Go to the documentation of this file.
52 #include "math_types.h"
157 typedef struct _MOTOR_Params_
192 #endif // end of MOTOR_LIB_H definition
@ OPERATE_MODE_SCALAR
V/f scalar control.
Definition: motor.h:99
SAMPLE_Mode_e
Enumeration for the estimator mode.
Definition: motor.h:109
@ MOTOR_CL_RUNNING
Definition: motor.h:130
@ MOTOR_RUN_FWC
Definition: motor.h:132
float32_t ratedFlux_Wb
Defines the rated flux, Wb.
Definition: motor.h:173
@ MOTOR_FAULT_STOP
Definition: motor.h:122
@ MOTOR_BRAKE_STOP
Definition: motor.h:123
@ MOTOR_IPD_HFI
Definition: motor.h:128
@ MOTOR_CTRL_RUN
Definition: motor.h:131
MOTOR_Status_e
Definition: motor.h:120
float32_t Rr_d_Ohm
Defines the direct rotor resistance, Ohm.
Definition: motor.h:167
@ MOTOR_CTRL_TORQUE_CW
(0100), CW spin with torque control
Definition: motor.h:145
FlyingStart_Mode_e
Enumeration for the Flying Start Mode.
Definition: motor.h:76
@ OPERATE_MODE_TORQUE
Torque control running mode.
Definition: motor.h:101
@ MOTOR_RS_RECALC
Definition: motor.h:134
@ MOTOR_TYPE_INDUCTION
induction
Definition: motor.h:68
@ MOTOR_CTRL_IDENTIFy
(1010), Motor parameters identification
Definition: motor.h:151
@ MOTOR_CTRL_FREQ_CW
(0010), CW spin with speed closed-loop (Hz)
Definition: motor.h:143
@ MOTOR_SEEK_POS
Definition: motor.h:126
@ MOTOR_CTRL_TORQUE_CCW
(0101), CCW spin with torque control
Definition: motor.h:146
float32_t Ls_d_H
Defines the direct stator inductance, H.
Definition: motor.h:164
@ SAMPLE_MODE_SDFM
sdfm
Definition: motor.h:115
@ MOTOR_CTRL_SPEED_CCW
(0111), CCW spin with speed closed-loop (rpm)
Definition: motor.h:148
@ SAMPLE_MODE_DCLINK
dclink_ss
Definition: motor.h:112
@ OPERATE_MODE_SPEED
Speed closed-loop running mode.
Definition: motor.h:102
@ MOTOR_CHARGE
Definition: motor.h:125
BRAKE_Mode_e
Enumeration for the braking Mode.
Definition: motor.h:86
@ FREE_STOP_MODE
Free stop mode without braking.
Definition: motor.h:87
@ SAMPLE_MODE_DCSS4
dclink_ss4
Definition: motor.h:111
MOTOR_Type_e type
Defines the motor type.
Definition: motor.h:159
@ MOTOR_IDENTIFICATION
Definition: motor.h:133
float32_t Rr_q_Ohm
Defines the quadrature rotor resistance, Ohm.
Definition: motor.h:168
float32_t Lmag_H
Defines the magnetizing inductance, H.
Definition: motor.h:163
MOTOR_Type_e
Enumeration for the motor types.
Definition: motor.h:67
@ SAMPLE_MODE_3LSR
three_shunt
Definition: motor.h:113
@ FLYINGSTART_MODE_STANDBY
Standby Mode.
Definition: motor.h:78
@ MOTOR_CTRL_URGENT_STOP
(1001), urgent stop
Definition: motor.h:150
@ OPERATE_MODE_POWER
Constant power running mode.
Definition: motor.h:103
@ MOTOR_STOP_IDLE
Definition: motor.h:121
@ MOTOR_CTRL_SPEED_CW
(0110), CW spin with speed closed-loop (rpm)
Definition: motor.h:147
float32_t Ls_q_H
Defines the quadrature stator inductance, H.
Definition: motor.h:165
@ MOTOR_CTRL_BRAKE_STOP
(0001), Stop the motor with braking mode
Definition: motor.h:142
@ MOTOR_NORM_STOP
Definition: motor.h:124
uint_least16_t numPolePairs
Defines the number of pole pairs.
Definition: motor.h:161
@ MOTOR_OL_START
Definition: motor.h:129
@ MOTOR_CTRL_FREQ_CCW
(0011), CCW spin with speed closed-loop (Hz)
Definition: motor.h:144
@ MOTOR_CTRL_DEBUG_CHECK
(1000), debug monitor
Definition: motor.h:149
@ DYNAMIC_BRAKE_MODE
N/A, Dynamic braking mode.
Definition: motor.h:90
@ SAMPLE_MODE_3INL
inline
Definition: motor.h:114
@ FLYINGSTART_MODE_HALT
Halt Mode.
Definition: motor.h:77
MOTOR_CtrlMode_e
Enumeration for the motor drive control state.
Definition: motor.h:140
@ HARDSWITCH_BRAKE_MODE
Hard switch braking mode.
Definition: motor.h:88
float32_t Rs_d_Ohm
Defines the direct stator resistance, Ohm.
Definition: motor.h:170
@ MOTOR_CTRL_FREE_STOP
(0000), Stop the motor with free mode
Definition: motor.h:141
Defines the motor parameters.
Definition: motor.h:158
@ SAMPLE_MODE_DCSS2
dclink_ss2
Definition: motor.h:110
@ MOTOR_ALIGNMENT
Definition: motor.h:127
@ MOTOR_TYPE_PM
permanent magnet
Definition: motor.h:69
float float32_t
Definition: dcl_common.h:58
@ REGENERATION_BRAKE_MODE
N/A, Regeneration braking mode.
Definition: motor.h:91
@ OPERATE_MODE_VQCL
Vq direction control.
Definition: motor.h:100
OPERATE_Mode_e
Enumeration for the control mode.
Definition: motor.h:98
@ MOTOR_CTRL_RSCALC
(1011), Rs recalculation
Definition: motor.h:152
@ FORCESTOP_BRAKE_MODE
Force alignment braking mode.
Definition: motor.h:89
float32_t Rs_q_Ohm
Defines the quadrature stator resistance, Ohm.
Definition: motor.h:171