AM243x Motor Control SDK  09.02.00

Introduction

Contains Enhanced SMO Estimator (ESMO) functions implementation.

Go to the source code of this file.

Data Structures

struct  ESMO_Handle
 Defines the ESMO controller object. More...
 

Macros

#define ESMO_inline_run   ESMO_run
 

Functions

ESMO_Handle ESMO_init (void *pMemory, const size_t numBytes)
 Initializes the ESMO controller. More...
 
void ESMO_updateFilterParams (ESMO_Handle handle)
 Reset the ESMO controller. More...
 
void ESMO_updatePLLParams (ESMO_Handle handle)
 Reset the ESMO controller. More...
 
void ESMO_full_run (ESMO_Handle handle, float32_t Vdcbus, MATH_vec3 *pVabc_pu, MATH_vec2 *pIabVec)
 Runs the any actions that user desires on top of ESMO controller. More...
 
static void ESMO_run (ESMO_Handle handle, const float32_t Vdcbus, MATH_vec3 *pVabc_pu, MATH_vec2 *pIabVec)
 Runs the ESMO controller. More...
 
static void ESMO_resetParams (ESMO_Handle handle)
 Reset the ESMO controller. More...
 
void ESMO_setParams (ESMO_Handle handle, const USER_Params *pUserParams)
 Set the ESMO controller. More...
 
static void ESMO_setPLLParams (ESMO_Handle handle, const float32_t pll_KpMax, const float32_t pll_KpMin, const float32_t pll_KpSF)
 Set PLL parameters for the ESMO controller. More...
 
static void ESMO_setPLLKi (ESMO_Handle handle, const float32_t pll_Ki)
 Set PLL parameters for the ESMO controller. More...
 
static void ESMO_setBEMFThreshold (ESMO_Handle handle, const float32_t bemfThreshold)
 Set bemfThreshold for the ESMO controller. More...
 
static void ESMO_setPLLKpSF (ESMO_Handle handle, const float32_t pll_KpSF)
 Set kp of the pll for the ESMO controller. More...
 
static void ESMO_setKslideParams (ESMO_Handle handle, const float32_t KslideMax, const float32_t KslideMin)
 Set PLL parameters for the ESMO controller. More...
 
static void ESMO_setKslide (ESMO_Handle handle, const float32_t Kslide)
 Sets Kslide for the ESMO controller. More...
 
static void ESMO_resetPLL (ESMO_Handle handle)
 Resets PLL integration for the ESMO controller. More...
 
static void ESMO_setOffsetCoef (ESMO_Handle handle, const float32_t offsetSF)
 Sets angle offset coefficient for the ESMO controller. More...
 
static void ESMO_setBEMFKslfFreq (ESMO_Handle handle, const float32_t filterFc_sf)
 Sets speed filter cut off frequency for the ESMO controller. More...
 
static void ESMO_setSpeedFilterFreq (ESMO_Handle handle, const float32_t lpfFc_Hz)
 Sets speed filter cut off frequency for the ESMO controller. More...
 
static void ESMO_setPLLKp (ESMO_Handle handle, const float32_t pll_Kp)
 Runs the ESMO controller. More...
 
static void ESMO_setAnglePu (ESMO_Handle handle, const float32_t theta_rad)
 Set Angle to the ESMO controller. More...
 
static void ESMO_setPLLSpeedPu (ESMO_Handle handle, const float32_t speed_Hz)
 Set Angle to the ESMO controller. More...
 
static void ESMO_setSpeedRef (ESMO_Handle handle, const float32_t speedRef_Hz)
 Set reference speed to the ESMO controller. More...
 
static float32_t ESMO_getSpeed_Hz (ESMO_Handle handle)
 Gets the speed from the ESMO controller. More...
 
static float32_t ESMO_getSpeedPLL_Hz (ESMO_Handle handle)
 Gets the PLL speed from the ESMO controller. More...
 
static float32_t ESMO_getAnglePLL (ESMO_Handle handle)
 Gets the PLL angle from the ESMO controller. More...
 
static float32_t ESMO_getAngleElec (ESMO_Handle handle)
 Gets the angle from the ESMO controller. More...
 
static void ESMO_updateKslide (ESMO_Handle handle)
 Update Kslide for the ESMO controller. More...